The configuring example is intended for precise and fast
control of processes subject to strong interference. The interference must be
known to the user and must be measured. An example project is used to illustrate
implementation and potential for improvement in comparison with a basic PID controller.
The example deals with the following main topics:
Creating an instance of the measuring point
Determining the measured data required for the model
draft
Identification using the MPC configurator
Example simulation with/without feedforward control
to demonstrate the potential benefit
Download