|
Integral Path Interpolation for Handling Modules in
Packaging Machines
Handling – this means free movement in a space mainly
between variable start and end points. The interpolation for handling processes
integrated in the SIMOTION Motion Control System optimizes the performance and
productivity of machines. The path interpolation technology object reduces the
system load decisively and thus increases the performance of a machine. Only
one controller is required for all machine functions. The technology object can
be used together with the SIMOTION Top Loading software library.
more |
SIMOTION V4.1 and PROFINET for High Performance
in Machine Automation
Version 4.1 of the SIMOTION Motion Control System features
extended
PROFINET functions for modular machine concepts, enabling electrical
and hydraulic drives to be synchronized with each other. In addition, controllers
can be configured simultaneously at the same PROFINET interface as IO Controller
and IO Device. By means of controller-controller communication via PROFINET,
SIMOTION V4.1 permits axis synchronization between several controllers. |
Interpolation in the SIMOTION Runtime System
Interpolation
in the runtime system of SIMOTION V4.1 supplements the existing applicative interpolation via cams. The functionality
is platform-independent and offers polynomial interpolation in addition to linear
and circular interpolation. An important area of application is the handling
of products. For this purpose, various transformations were implemented for conventional
kinematics such as portal, SCARA, roll, jointed arm or delta kinematics. |
New PC-based Motion Control System SIMOTION P350
The constantly increasing demands on the performance and
flexibility of automation solutions can now be met by the new
PC-based SIMOTION P350-3 Motion Control System, which integrates logic, motion control and HMI
functionalities in an industry-standard box PC. The PC solution is open to be
used with additional hardware and software and offers twice the level of performance
of its predecessor. |
New, High-performance Controller SIMOTION C240
The C240 Controller offers a 2.5 times increase in performance
compared to the C230 Controller. As many as 32 axes can be coordinated by means
of PROFIBUS with PROFIdrive-Profile. The retained data and the working memory
capacities have been expanded to 100 KB and 20 MB respectively. The installation
and interfaces of the C240 are fully compatible with the C230-2. The C240 Controller
has four encoders and four analog interfaces for connection of analog drive units
or stepper drives with pulse/direction interface, making it also particularly
suitable for retrofit applications.
|