Technical Forum

SIMATIC S7-400 / S7-400H / S7-400F /FH

2oo3 Voting

Thread Starter: MadmanK   Started: 9/18/2008 9:27 PM   Replies: 2

« Previous thread Next thread »
Page 1 of 1 (3 items)
  9/18/2008, 9:27 PM
Joined 10/2/2007
Last visit: 1/28/2015
Posts: 2
Rating:
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
My customer wants 2oo3 voting on redundant signals to SIL3. Using an S7-400FH, will I have to carry out the voting within the safety programme (as I can only find 1oo2 within the I/O module directly)? They want 2oo3 for all digital and analogue signals.

I realise the F-Systems library has a boolean 2oo3 Vote function (for BOOLS only) but how do I configure the I/O module to maintain SIL3?

Any advice would be appreciated...
Top
  9/18/2008, 10:46 PM
Joined 8/17/2007
Last visit: 10/3/2013
Posts: 488
Rating:
Rated: Excellent [4.31 out of 5 / rated 35 time(s)]. (35) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Which version F block are you using? As per manual F-library V1.2 has  F_2oo3_R block.

Please see the page from manual attached.

But  F option pack 6.0 has library 1.3
This shoul have following voting blocks

Overview

Block name

Block number

Description

F_2oo3DI

FB 316

2oo3 evaluation of inputs of data type BOOL with discrepancy analysis

F_2oo3AI

FB 317

2oo3 evaluation of inputs of data type REAL with discrepancy analysis

F_1oo2AI

FB 318

1oo2 evaluation of inputs of data type REAL with discrepancy analysis

 



Also see the link to manual
http://support.automation.siemens.com/WW/view/en/2201072

In this manual

Attachment: Acceptance test of F-Block types.pdf  (83 Downloads)

Jomy M Jose
Jacobs Engineering Group Inc.
111 Corning Rd., Suite 200
Cary, NC 27518, USA

Top
  9/19/2008, 10:06 AM
Joined 10/2/2007
Last visit: 1/28/2015
Posts: 2
Rating:
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 

Thank you for the heads up, I was reading an (much) earlier version of the manual by mistake.

Top
Page 1 of 1 (3 items)
Actions