Technical Forum

MICROMASTER

Analog Outputs Micromaster 440

Thread Starter: Da Monsta   Started: 5/27/2008 1:26 PM   Replies: 2

« Previous thread Next thread »
Page 1 of 1 (3 items)
  5/27/2008, 1:26 PM
Joined 5/19/2008
Last visit: 5/27/2008
Posts: 3
Rating:
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Hello,

We are two french students and we would like to use analog outputs of the Micromaster in order to display the motor speed. We need to get a proportional voltage beetween 0-24V.

If somebody could help us grin

Regards

Top
  5/28/2008, 8:42 AM
Joined 5/7/2008
Last visit: 1/22/2015
Posts: 41
Rating:
Rated: Outstanding [3.5 out of 5 / rated 2 time(s)]. (2) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Hello!

It isn't possible to make 0-24V analog signal directly from MICROMASTER, You must use converter signal 0-10V/0-24V or similiar.
Top
  6/4/2008, 6:11 PM
Joined 3/27/2008
Last visit: 9/2/2014
Posts: 156
Rating:
Rated: Excellent [4.14 out of 5 / rated 7 time(s)]. (7) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
The analogue output is controlled by Paramater P0771, here you will find 'in000' and 'in001'.
So parameter p0771, in000 should be set to 21 for output frequency.

This output is 0/20ma, available at terminals 12 & 13. If you need to have a Voltage output put a 500 Ohm, (470 Ohm is more readilly available), into terminals 12 and 13. This will provide 10 Volts proportional to frequency or speed, across the resistor.

At 50Hz you will have 10 Volts, 0 Hz 0 Volts.

I know this is not 24 Volts but as close as I can get........

T.
Top
Page 1 of 1 (3 items)
Actions