Technical Forum

Industrial Controls

Sirius Motor Starter Contactors - 3RT

Thread Starter: Crego   Started: 5/1/2008 6:19 PM   Replies: 10

« Previous thread Next thread »
12» Page 1 of 2 (11 items)
  5/1/2008, 6:19 PM
Joined 5/1/2008
Last visit: 5/16/2008
Posts: 3
Rating:
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
I just purchased 4 of these Motor Starters Part# 3RT 1065-6AB36

and they won't pull in unless I tap on the contactors on the side.  I have to do this every time I apply power to it.   My wire connections are clean, so I don't know what the problem is.  If I was having a problem with only one of the starters I would think it was on my end, but since all 4 are giving me the same problem, I am wondering if it's a design issue?  Any solutions to this problem?
Top
  5/2/2008, 5:50 AM
Joined 11/13/2007
Last visit: 5/25/2013
Posts: 134
Rating:
Rated: Excellent [4.5 out of 5 / rated 2 time(s)]. (2) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
hi. Check supply voltage to contactor it should be 24 V. DC
Top
  5/2/2008, 1:12 PM
Joined 5/2/2008
Last visit: 5/2/2008
Posts: 1
Rating:
Rated: Excellent [5 out of 5 / rated 1 time(s)]. (1) 
Rated: Excellent [5 out of 5 / rated 1 time(s)]. (1) 

Hello Crego,

DC-Power supply must be able to supply 27A for a duration of max 95ms until contactor is closed.

Please find attached a copy of technical data for contactors 3RT106.

Best regards

Paparazzo


Attachment: technical data 3RT106.pdf  (39 Downloads)



=== Edited by Paparazzo @ 5/2/2008 1:12 PM [GMT ] ===



Top
  5/2/2008, 4:22 PM
Joined 5/1/2008
Last visit: 5/16/2008
Posts: 3
Rating:
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Thanks for the comments. 
I'm using a 40A  24V DC power supply. I'm wondering if there is a problem with the actual contactors not closing properly on the motor starters.  It doesn't make sense to me why it pulls in after i tap the contactor with the fat end of the screw driver.    
 
Thank you for the data sheet.
Top
  5/3/2008, 9:23 AM
Joined 11/13/2007
Last visit: 5/25/2013
Posts: 134
Rating:
Rated: Excellent [4.5 out of 5 / rated 2 time(s)]. (2) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
hi Crego. if you still have problem-make shure (use Ohm Meter)that your contactor A1 and A2 contacts for magnetic coil do not broken. It is strange that all 3 contactors have the same problem-may be connection wrong? And -for answer why contactor tap keep closed after when you push it down-because current which going thrue contacts creat force  to hold it closed.
regards
Top
  5/5/2008, 5:17 PM
Joined 5/1/2008
Last visit: 5/16/2008
Posts: 3
Rating:
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Thank you Kanan, I will try that this week and post my results.
Top
  9/24/2009, 4:07 PM
Joined 9/24/2009
Last visit: 9/24/2009
Posts: 1
Rating:
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
We have a similar problem with a 3RT1044 contactor
Top
  9/25/2009, 8:38 AM
Joined 11/27/2006
Last visit: 2/28/2011
Posts: 37
Rating:
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
27A :lolz

I assume this is only for the extra large contactors.
Top
  5/20/2014, 6:21 PM
Joined 2/12/2013
Last visit: 7/26/2014
Posts: 203
Rating:
Rated: Outstanding [3.62 out of 5 / rated 21 time(s)]. (21) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Paparazzo wrote:

Hello Crego,

DC-Power supply must be able to supply 27A for a duration of max 95ms until contactor is closed.

Please find attached a copy of technical data for contactors 3RT106.

Best regards

Paparazzo


HI there

Is this the the holding current rating or the closing current rating?as the VA requirement is different in the case of closing & holding.
Top
  5/21/2014, 7:32 AM
Joined 7/3/2013
Last visit: 6/14/2014
Posts: 232
Rating:
Rated: Outstanding [3.33 out of 5 / rated 76 time(s)]. (76) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Crego wrote:
I just purchased 4 of these Motor Starters Part# 3RT 1065-6AB36

and they won't pull in unless I tap on the contactors on the side.  I have to do this every time I apply power to it.   My wire connections are clean, so I don't know what the problem is.  If I was having a problem with only one of the starters I would think it was on my end, but since all 4 are giving me the same problem, I am wondering if it's a design issue?  Any solutions to this problem?


Dear Crego,

Thanx for your post,if you still facing this prblem then you have to contact to your vendor from whom to buy this product they will check the product if its realy a faulty then they must have to replace the same.
thumb
Regards

"It’s better to give than to receive. Especially advice"
Top
Thank you for this post from:
12» Page 1 of 2 (11 items)
Actions