Technical Forum

SIMATIC WinCC

WINCC Component Object Manager

Thread Starter: davism   Started: 4/28/2008 11:27 AM   Replies: 4

« Previous thread Next thread »
Page 1 of 1 (5 items)
  4/28/2008, 11:27 AM
Joined 4/21/2008
Last visit: 5/1/2008
Posts: 7
Rating:
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Hi everyone, I'm trying to import an S7 project from a vendor and am getting a message stating that WinCC (component object manager) software package is not installed. Is this a separate package to WinCC flexible 2007 advanced/runtime..?

I've looked on both DVDs and cannot see it as an install option. Do I need to purchase further software..?

Any help is much appreciated.
Martin

Attachment: wincc.JPG  (238 Downloads)

Top
  4/28/2008, 1:13 PM
Joined 11/9/2005
Last visit: 1/26/2015
Posts: 449
Rating:
Rated: Outstanding [3.83 out of 5 / rated 23 time(s)]. (23) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Hi

Yes there is a difference between WinCC and WinCC flexible .WinCC is the bigger brother of wincc flexible the two are not quite compatable or the same the structure is different .

The component object manager is part of wincc , I think ,most possible is that wincc is not installed on your PC, this will not stop you from working with the PLC.

Eric

Here we only work on 'no need to know basis' ,just fix whatever is wrong
Top
  4/28/2008, 8:56 PM
Joined 4/28/2008
Last visit: 11/14/2012
Posts: 2
Rating:
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 

There are several options in the installation of WinCC that need to be selected for an integrated project.

  • Object Manager - This allows the insertion of the WinCC objects into Simatic Manager
  • AS-OS Engineering - This is the actuall tag/messages transfer mechanism
  • S7 Symbol Server - Allows you to 'browse' for S7 tags that have not yet been created within the WinCC project.

You can also add these options later by clicking add/remove components for WinCC.

Top
  4/29/2008, 8:53 AM
Joined 4/21/2008
Last visit: 5/1/2008
Posts: 7
Rating:
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 

Thanks everyone - seems I'm going to have to buy WinCC on  top of WinCC Flex cry

Martin

Top
  4/29/2008, 9:21 AM
Joined 9/7/2007
Last visit: 1/20/2015
Posts: 448
Rating:
Rated: Outstanding [3.67 out of 5 / rated 43 time(s)]. (43) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
if there are no changes to be applied in the SCADA system integrated in the project you need not Install the software you can edit the changes simply in the Simatic manager

Best Regards
Top
Page 1 of 1 (5 items)
Actions