Technical Forum

SINUMERIK CNC automation systems

sinumerik 810D stop ' NO Mode group Ready'

Thread Starter: almostafa   Started: 4/16/2008 11:17 PM   Replies: 5

« Previous thread Next thread »
Page 1 of 1 (6 items)
  4/16/2008, 11:17 PM
Joined 4/16/2008
Last visit: 4/25/2014
Posts: 20
Rating:
Rated: Very Good [2 out of 5 / rated 1 time(s)]. (1) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Dear friends
 I have a problem with my CNC punching machine .I use Sinumerik  MMC 103  .
When I try to make reference for the axies . I have this mesage
        " Stop: no group Mode ready"
I press the Reset button , and try again , the neassage is displayed .
please can any one tell me what this mean

best regards



=== Edited by almostafa @ 4/17/2008 9:34 AM [GMT ] ===


=== Edited by almostafa @ 4/17/2008 9:30 AM [GMT ] ===


Top
  4/18/2008, 2:33 PM
Joined 3/13/2008
Last visit: 3/31/2014
Posts: 55
Rating:
Rated: Outstanding [4 out of 5 / rated 2 time(s)]. (2) 
Rated: Excellent [5 out of 5 / rated 1 time(s)]. (1) 

Please check the diagnosis  screen, due to some nck-plc signal interlock – it is appearing. Please cross check the basic interlocks which should satisfy before starting Reference. I think m/c is running at JOG mode. Please revert back.


Regards,
Sanjoy
Top
  4/19/2008, 12:14 PM
Joined 4/16/2008
Last visit: 4/25/2014
Posts: 20
Rating:
Rated: Very Good [2 out of 5 / rated 1 time(s)]. (1) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Dear Sanjoy 
 Thank you at first , now when I measure the 24 v signal from FMN-C to the drives to enable the drives , the 24 v is missing . some times 24 V became present at the drive , and at this moment , every thing is ok . the problem was happend before on a long intervals , now it is repated so much , do you think the FMN-C is faulty , or it needs some signals to work properly.
what arew the interlcks for the FMN-C 
  Mostafa
Top
  4/20/2008, 11:52 AM
Joined 4/16/2008
Last visit: 4/25/2014
Posts: 20
Rating:
Rated: Very Good [2 out of 5 / rated 1 time(s)]. (1) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
 Dear all
  can any one tell about a link for the wiring digram for the FMNC , NCU 570 . the problem still exist , but some times system work for a short time , then stop.



=== Edited by almostafa @ 4/20/2008 2:00 PM [GMT ] ===


Top
  4/20/2008, 6:27 PM
Joined 4/16/2008
Last visit: 4/25/2014
Posts: 20
Rating:
Rated: Very Good [2 out of 5 / rated 1 time(s)]. (1) 
Rated: Very Good [2 out of 5 / rated 1 time(s)]. (1) 
  Now , its Ok , there one channel missing of one the the machine position Encoders.the wire was disconnected , but are there any alarm should be declared for this fault ? .
Top
  6/24/2008, 9:51 AM
Joined 9/27/2007
Last visit: 9/11/2009
Posts: 71
Rating:
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Yes, there is one alarm Number  300504 and 25000.In normal status, we use 300504 and 25000 for axis encoder alarm.If the encoder was fault or the calbe fault or the module interface fault,then the asix alarm that measuring system no active.

maybe in you system there is no alarm number, you should contact with OEM.
Top
Page 1 of 1 (6 items)
Actions