Technical Forum

SIMATIC S7-300 / S7-300F

CPU 315 - 2 DP

Thread Starter: Wave   Started: 11/15/2007 6:01 AM   Replies: 4

« Previous thread Next thread »
Page 1 of 1 (5 items)
  11/15/2007, 6:01 AM
Joined 4/23/2007
Last visit: 4/3/2014
Posts: 56
Rating:
Rated: Very Good [1.67 out of 5 / rated 3 time(s)]. (3) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
I dont see 2 DP ports on this CPU. There's only a MPI port, not a MPI/DP port. If this MPI port is not configurable as DP port then why the "- 2 DP" in its name? 

Regards,
Wave

"There is no spoon."
Top
  11/15/2007, 9:05 AM
Joined 4/24/2006
Last visit: 1/30/2015
Posts: 5736
Rating:
Rated: Excellent [4.21 out of 5 / rated 564 time(s)]. (564) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Hello Wave,

Well the number 2 stands for two ports. Depending on the used CPU 315-2DP, one is a MPI port and the second is a Profibus port.

When you have CPU315-2DP: 6ES7 315-2EH13-0AB0, you have a MPI/DP port and a DP port.

Best regards,

Wizard
Top
  11/19/2007, 10:34 AM
Joined 9/28/2005
Last visit: 1/9/2015
Posts: 412
Rating:
Rated: Outstanding [3.68 out of 5 / rated 28 time(s)]. (28) 
Rated: Good [1 out of 5 / rated 1 time(s)]. (1) 
Wizard wrote:
Hello Wave,

Well the number 2 stands for two ports. Depending on the used CPU 315-2DP, one is a MPI port and the second is a Profibus port.

When you have CPU315-2DP: 6ES7 315-2EH13-0AB0, you have a MPI/DP port and a DP port.

Best regards,

Wizard


Hi,

I think you mean:
[qoute]
When you have CPU315-2DP: 6ES7 315-2EH13-0AB0, you have a MPI/DP port and a Profinet/Ethernet port.
[/qoute]

Smurf


"The only difference between a problem and a solution is that people understand the solution."
Top
  11/19/2007, 10:40 AM
Joined 9/28/2005
Last visit: 1/9/2015
Posts: 412
Rating:
Rated: Outstanding [3.68 out of 5 / rated 28 time(s)]. (28) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Wave wrote:
I dont see 2 DP ports on this CPU. There's only a MPI port, not a MPI/DP port. If this MPI port is not configurable as DP port then why the "- 2 DP" in its name? 

Regards,
Wave


Hi,

Even more fun:

Take the CPU417-4H. Running through the text you will notice that the CPU has only 2 ports for DP and/or MPI. laugh
What happend to the other 2 ports? Simple, they are used for synchronization with the other CPU in the H-system. astonished

Smurf


"The only difference between a problem and a solution is that people understand the solution."
Top
  11/19/2007, 11:40 AM
Joined 4/24/2006
Last visit: 1/30/2015
Posts: 5736
Rating:
Rated: Excellent [4.21 out of 5 / rated 564 time(s)]. (564) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Hi Smurf,

Yes, You are right, thank you for your comment. blush

Best regards,

Wizard
Top
Page 1 of 1 (5 items)
Actions