Technical Forum

SIMATIC TDC, FM458, T400

SIMADYN-D controller

Thread Starter: PLalit   Started: 11/12/2007 8:33 PM   Replies: 1

« Previous thread Next thread »
Page 1 of 1 (2 items)
  11/12/2007, 8:33 PM
Joined 11/12/2007
Last visit: 9/2/2014
Posts: 1
Rating:
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Dear All,

I am very new user for  Simadyn -D controller, need to convert / edit  logic written in SIM D (Struc View ) controller into new controller.

. Does anybody has soft copy of the instruction set / link for its manual?

. What are the meanings of the blocks and instructions?

. How to download and edit the code?

. which softwares are to be used?

. Does it opens in simatic manager ?

Thanks in advance fro the reply
Top
  11/16/2007, 6:26 PM
Joined 8/31/2005
Last visit: 1/30/2015
Posts: 1196
Rating:
Rated: Outstanding [3.84 out of 5 / rated 146 time(s)]. (146) 
Users with special expertise supervising conferences
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 

Hello,

SIMADYN D is in phase out state and should not be used for new projects.

Actual products and similar to SIMADYN D are T400 (for Masterdrives) FM458 (for S7-400) and SIMATIC TDC.

Older SIMADYN D sations were programmed with STRUC L or STRUC G.
The files are CFP, CMP, UFP, UMP, OFP, OMP.

Newer ones used STEP 7, CFC and D7-SYS.
The file is a Step7 Archive (ARJ or ZIP)


It would help me a lot if you can say which SIMADYN D Processor you have (eg. PM16, PM5, PT16, PT31 etc) to replace and what you plan to use instead of it.


mfG / Best Regards

Dirk
Top
Page 1 of 1 (2 items)
Actions