Technical Forum

SIMATIC S7-200

V4.0 STEP 7 MicroWIN SP3

Thread Starter: yanco   Started: 10/24/2007 11:14 AM   Replies: 3

« Previous thread Next thread »
Page 1 of 1 (4 items)
  10/24/2007, 11:14 AM
Joined 8/27/2007
Last visit: 3/26/2010
Posts: 8
Rating:
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Hi !
I have  installed V4.0 STEP 7 MicroWIN SP3  on computer with windows vista operating system, but the program is not working.
 Does anyone have the same problem ?
greetingy , Y
Top
  10/24/2007, 11:29 AM
Joined 7/24/2006
Last visit: 1/28/2015
Posts: 2267
Rating:
Rated: Outstanding [3.79 out of 5 / rated 289 time(s)]. (289) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Hi,

goto your HD and browse to the Microwin.exe file.

Enable the file, press the right mouse button and open the properties´.

Here you can find a tap named "Compatibility"´. Now select WindowsXP mode and try. This may work.

I do not know if there are limitation (Multimaster mode, Ethernet, USB-2-RS232 converter, .....).

Basically the actuall MicroWIN version is not supporting Microsoft Vista.

Regards

Helmut
Top
  11/2/2007, 2:54 PM
Joined 9/28/2005
Last visit: 1/9/2015
Posts: 412
Rating:
Rated: Outstanding [3.68 out of 5 / rated 28 time(s)]. (28) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Hi,

I heard a rumour about Vista and Micro/Win V4.0 SP6 which should be compatible.

And as you can see, Micro/Win V4 SP3 is not up-to-date anymore, SP5 can be downloaded from here.

Smurf


"The only difference between a problem and a solution is that people understand the solution."
Top
  11/3/2007, 2:49 AM
Joined 11/3/2007
Last visit: 11/3/2007
Posts: 1
Rating:
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Hi guys,

I new here but I discovery something that may help you.

I did my STEP 7 MicroWin V3.2 run under my Windows Vista.

First right click "microwin.exe", that must be at C:\Program Files\Siemens\STEP 7-MicroWIN\Bin\;
Go to Properties;
Compatibility;
and there is what I did, check "Run this program in compatibility mode for:" and than choose "Windows XP (Service Pack 2)".

Finaly I checked "Run this program as an administrator" and this made my STEP7 okay.

My problem was that he couldn't read the file S7ONLINX.dll

I wish it helps you.

Hugs from BRAZIL!
laugh
Top
Page 1 of 1 (4 items)
Actions