Technical Forum

SIMATIC WinCC (TIA Portal)

Create discrete alarms in Tia portal V11

Thread Starter: MrBin   Started: 12/6/2013 5:43 AM   Replies: 3

Tags TIA WinCC Adv Alarms Messages

« Previous thread Next thread »
Page 1 of 1 (4 items)
  12/6/2013, 5:43 AM
Joined 3/23/2011
Last visit: 1/14/2015
Posts: 41
Rating:
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Hi everybody!
I have a KTP400 Panel. I want to create a discrete alarm, example: when "START" button is pushed, alarm text displays "Machine Starts". But I can't do that. Hope getting your helps!
Thanks everybody!
Top
  12/6/2013, 6:55 AM
Joined 1/21/2013
Last visit: 1/27/2015
Posts: 2006
Rating:
Rated: Excellent [4.1 out of 5 / rated 114 time(s)]. (114) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Hi MrBin,
Take a look, this is an example for alarm messages:
http://support.automation.siemens.com/WW/view/en/62121503
Top
  12/7/2013, 8:22 AM
Joined 3/23/2011
Last visit: 1/14/2015
Posts: 41
Rating:
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Thanks Ste39!
I read Wincc_TIA_alarm document. In Configuration of discrete alarms section, types of data for trigger tag are int, word, uint but type of my tag for alarm is bool. I don't understand that. Can you explain for me!
Top
  12/7/2013, 10:01 AM
Joined 1/21/2013
Last visit: 1/27/2015
Posts: 2006
Rating:
Rated: Excellent [4.1 out of 5 / rated 114 time(s)]. (114) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Hello MrBin,
You can select a variable of type WORD and specify the trigger BIT of the WORD.
or
You can convert the discrete alarms at PLC to a WORD or UINT and transfer to a HMI.
If you have more than 16 alarms you have to create a new WORD or UINT and trasfer to HMI.
maybe this can help you:
How can you group separate signals (variables of the "Bool" data type) to one variable of the "Word" type and again extract them from that "Word" variable (Bool - Word data type conversion)?



=== Edited by Ste39 @ 12/9/2013 5:59 AM [GMT ] ===


=== Edited by Ste39 @ 12/7/2013 10:24 AM [GMT ] ===


Top
Page 1 of 1 (4 items)
Actions