Technical Forum

SINAMICS

Downloading from starter to SINAMICS S120 CU 320

Thread Starter: Miki Rapaic   Started: 8/26/2007 8:49 PM   Replies: 6

« Previous thread Next thread »
Page 1 of 1 (7 items)
  8/26/2007, 8:49 PM
Joined 12/28/2006
Last visit: 10/18/2014
Posts: 42
Rating:
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Hiblush

I have a problem concerning sinamics S 120 and starter software....
I'm using starter software 4.0.. and with this i created my project...


The problem is next:
I'm trying to load this project to CU 320 using RS 232 port but I can't establish the
communication ...
I tried  with RS 232 cable, PG/PC settings (USS...) but i couldn't get it right....
My questions are next:
Which cable should I use  ...?
What should I set for PG/PC (USS) ??
What transfer rate should i set (9600) ??
We wont to use PROFIBUS communication  after we download project (is this a problem) ?
Do I have to set anything else on S 120 or Starter 4.0 before going online ?
Is there anything elese to do or set ???

I hope someone can help me with this, i really need this informations....

P.S
Strange, we prepared entire project and we can't do anything before we fix this grincry
And our provider said we could download this just fine using RS 232 port and cable we used with G 110
Top
  8/27/2007, 4:07 AM
Joined 4/26/2007
Last visit: 1/20/2014
Posts: 133
Rating:
Rated: Outstanding [3.82 out of 5 / rated 11 time(s)]. (11) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Sorry I could not attach the application guide for this but site kept erroring on me when I tried to upload.  This is the just of it.  I have done this before and found it slow compared to Profibus for connection to CU310 or CU320.  A null modem cable is what I used.
1. In STARTER, from Project > Set PC/PG interface, select the Serial cable (PPI) interface. If this is not available from the dropdown list, you first have to add it using Select. Note: If the interface cannot be added to the selection menu, the driver for the serial interface has to be installed. The STARTER must not be active when installing the driver. 
2. Enter the following settings. The "0" address and the transmission rate of 19.2 kbit/s are important here.    
3. On CU310/CU320, set bus address "3" on the Profibus address switch.
4. When setting up the drive unit, also set bus address "3". Note: The bus addresses on CU310/CU320 and on the PC must not be set the same.     
5. G150: The connecting cable from CU320 to AOP30 must be ground off on CU320. A null modem cable must be connected up here as a link between the PC (COM interface) and CU320. This interface must not be changed.
Top
  8/27/2007, 8:22 AM
Joined 8/23/2007
Last visit: 9/24/2013
Posts: 56
Rating:
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Hai Mr.Miki,

I think Sinamics RS232 only for Operator display. For Starter commissioning Either Profibus or Ethernet via you have to do the commissioning.

Bye..
Top
  8/27/2007, 2:25 PM
Joined 4/26/2007
Last visit: 1/20/2014
Posts: 133
Rating:
Rated: Outstanding [3.82 out of 5 / rated 11 time(s)]. (11) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Since V2.4 firmware and V4.0 STARTER you can connect and program via the RS232 port.

Attachment: RS232Connection.pdf  (593 Downloads)

Top
  8/27/2007, 10:54 PM
Joined 10/19/2005
Last visit: 5/9/2010
Posts: 272
Rating:
Rated: Outstanding [4 out of 5 / rated 21 time(s)]. (21) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 

Hello Miki,

Here is a link to some information that I've used successfully to connect via RS-232 to a CU320 in my S120 drive:  http://support.automation.siemens.com/WW/view/en/23963280

This works nicely.

Hope this helps...

Top
  6/6/2012, 5:23 PM
Joined 3/19/2012
Last visit: 4/10/2014
Posts: 2
Rating:
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
for communication between PG/PC and drive I think RS232 cable is required and co called zero modem cable that means cross over cable 

Attachment: Panel_Kommunikation_Steckerbelegung_T1_01_e.pdf  (209 Downloads)

Top
  7/12/2013, 2:44 PM
Joined 9/1/2005
Last visit: 2/1/2015
Posts: 2935
Rating:
Rated: Excellent [4.03 out of 5 / rated 132 time(s)]. (132) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
new question split to seperate thread Can not connect my laptop to CU320 via USB-RS232 converter.

Best regards
CS Moderator
Top
Page 1 of 1 (7 items)
Actions