Technical Forum

SIMATIC WinCC (TIA Portal)

comfort panel ktp400 to s7-300 step7 v5.5 sp2

Thread Starter: Rene Schouten   Started: 8/3/2013 10:15 AM   Replies: 2

Tags HMI-Migration

« Previous thread Next thread »
Page 1 of 1 (3 items)
  8/3/2013, 10:15 AM
Joined 7/3/2012
Last visit: 10/31/2014
Posts: 5
Rating:
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Hello,

I want to connect a s7-315-2dp over profibus to a comfort panel ktp400. The problem is that
the cpu is in a step 7 v5.5 project and the KTP400 display in tia portal V12. My question is: Is this possible and how?

Thanks for the answer.
Top
  8/4/2013, 1:11 PM
Joined 5/28/2008
Last visit: 1/24/2015
Posts: 3288
Rating:
Rated: Outstanding [3.71 out of 5 / rated 598 time(s)]. (598) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Rene Schouten wrote:
Hello,

I want to connect a s7-315-2dp over profibus to a comfort panel ktp400. The problem is that
the cpu is in a step 7 v5.5 project and the KTP400 display in tia portal V12. My question is: Is this possible and how?

Thanks for the answer.
Hello,
KTP can be programmed using WinCC flexible as from version 2008 SP2.
Please see section 4.2 of the attached file.
So if you do not like to use TIA portal, you can use STEP 7  with WinCC flexible.
Hope this helps.

Attachment: WCFWhatsNewenUS.pdf  (75 Downloads)

Ayman Elotaify
MISC Egypt
www.miscegypt.com

Top
  8/6/2013, 11:27 AM
Joined 4/24/2006
Last visit: 1/23/2015
Posts: 5728
Rating:
Rated: Excellent [4.2 out of 5 / rated 560 time(s)]. (560) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Rene Schouten wrote:
Hello,

I want to connect a s7-315-2dp over profibus to a comfort panel ktp400. The problem is that
the cpu is in a step 7 v5.5 project and the KTP400 display in tia portal V12. My question is: Is this possible and how?

Thanks for the answer.
Hello Rene Schouten,

Yes, it's possible. laugh

Have a look at the following link:
Joint configuration with WinCC (TIA Portal) and STEP 7 V5.x

Best regards,

Wizard
Top
Page 1 of 1 (3 items)
Actions