Technical Forum

STEP 7 (TIA Portal)

upgrading from v11 to v12

Thread Starter: avtel   Started: 4/12/2013 12:57 PM   Replies: 2

« Previous thread Next thread »
Page 1 of 1 (3 items)
  4/12/2013, 12:57 PM
Joined 2/26/2013
Last visit: 1/21/2015
Posts: 26
Rating:
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
hello,
I have a question on the same issue - whats are the options of upgrading from v11 to v12? Is there necessary to buy programm completly or there is a option of lower price upgrading (lower then v12 cost)

thank you un advance


best regards



=== Edited by O_Moderator @ 4/12/2013 1:09 PM [GMT ] ===
new subject after splitting from will s7-1500 series be available in TiA portal V11 through hardware support packages? Or is an upgrade from V11 to V12 required?

Top
  4/12/2013, 1:56 PM
Joined 4/24/2006
Last visit: 1/27/2015
Posts: 5734
Rating:
Rated: Excellent [4.21 out of 5 / rated 562 time(s)]. (562) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Hello avtel,

Please have a look at the following link:
Which license do you need to upgrade from STEP 7 version V5.x, V10.5 or V11 to the TIA Portal V12?

If you already have a license for Step 7 v11, you can use an upgrade. (It's cheaper)

Best regards,

Wizard
Top
  4/12/2013, 2:39 PM
Joined 2/26/2013
Last visit: 1/21/2015
Posts: 26
Rating:
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 

thank you very much WIZARD!

best regards

Top
Page 1 of 1 (3 items)
Actions