Technical Forum

SINAMICS

PROBLEM AND FAULT IN SINAMICS CU320

Thread Starter: PEDRO R   Started: 12/4/2012 4:58 AM   Replies: 1

« Previous thread Next thread »
Page 1 of 1 (2 items)
  12/4/2012, 4:58 AM
Joined 7/27/2012
Last visit: 12/14/2013
Posts: 41
Rating:
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Hi my friends, I write to you because i have one problem with the sinamics CU320, ATTACH one image about the codes of error it shows me the screen.

you can see the CODE OF ERROR in the screen, But the description funny characters o letters. and i question how i do for repair the sinamics CU320. i have two CU320, CU1 and CU2, The CU2 have problems as you can see in the photo.


I also need to know what parameters I can tell if the encoder is failing or if the SINAMICS CU320 is damaged. and steps for testing.

please i need help

Attachment: IMG-20121203-00202.jpg  (74 Downloads)

Top
  12/4/2012, 4:56 PM
Joined 5/24/2012
Last visit: 12/2/2013
Posts: 6
Rating:
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Mr. Rosales,

you can have information about all faults and alarms in the List Manual.

S120/S150
http://support.automation.siemens.com/WW/view/en/59750648

Others
http://support.automation.siemens.com/WW/view/en/10804921/133300
(search for "list manual")


Best Regards.
Silvio Morais
Rnf:lblSmileyTooltip_santa
Top
Page 1 of 1 (2 items)
Actions