Technical Forum

Communication / Networks

Constructing a Profinet Network with s7 1200 and TPS-1 Profinet IO

Thread Starter: aachener_1   Started: 11/15/2012 4:20 PM   Replies: 7

« Previous thread Next thread »
Page 1 of 1 (8 items)
  11/15/2012, 4:20 PM
Joined 11/13/2012
Last visit: 2/12/2013
Posts: 8
Rating:
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 

Hello Forum,

As I wrote in the topic, I want to intagrate TPS-1 IO to S7 device catalog. That is why i ve installed the GSD files of TPS-1. But could not find the device in the catalog to constract a PROFINET Network.

I am quite new in the TIA V11. But this is the way to learn it.

My question is: How can I add this TPS-1 in the s7 device catalog in TIA V11 ?

Thanks in advance !
Top
  11/15/2012, 5:30 PM
Joined 7/7/2010
Last visit: 1/28/2015
Posts: 3594
Rating:
Rated: Excellent [4.05 out of 5 / rated 427 time(s)]. (427) 
Users with special expertise supervising conferences
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
aachener_1 wrote:

Hello Forum,

As I wrote in the topic, I want to intagrate TPS-1 IO to S7 device catalog. That is why i ve installed the GSD files of TPS-1. But could not find the device in the catalog to constract a PROFINET Network.

I am quite new in the TIA V11. But this is the way to learn it.

My question is: How can I add this TPS-1 in the s7 device catalog in TIA V11 ?

Thanks in advance !

When you are showing these views, does your TPS-1 appear in the list on the right (see attached image)?

Attachment: HW_Catalog_s7-1200.jpg  (56 Downloads)

Helpful? Rate it.
Solved? Post it.
http://geo.co/s/Wmdn

Top
Thank you for this post from:
  11/16/2012, 2:17 PM
Joined 8/31/2010
Last visit: 1/27/2015
Posts: 1486
Rating:
Rated: Excellent [4.01 out of 5 / rated 154 time(s)]. (154) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
aachener_1 schrieb:

Hello Forum,

As I wrote in the topic, I want to intagrate TPS-1 IO to S7 device catalog. That is why i ve installed the GSD files of TPS-1. But could not find the device in the catalog to constract a PROFINET Network.

I am quite new in the TIA V11. But this is the way to learn it.

My question is: How can I add this TPS-1 in the s7 device catalog in TIA V11 ?

Thanks in advance !


Hello aachener_1,

assuming you have successfully installed the GSDML in TIA Portal v11.

You find your device under Other field devices -> PROFINET IO -> Gateway / Drives / any other suitable category (I hope the search function will also work here)

Like it? Rate it!
Top
Thank you for this post from:
  11/16/2012, 9:25 PM
Joined 11/13/2012
Last visit: 2/12/2013
Posts: 8
Rating:
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 

Thanks a lot Huggy and Ganes !

I just made unnecessary panic. It was there, i found it. Now i have to construct my network. In order to do that i need to get used to TIA V11.

Afterwards  the task is the connectin TPS-1 with IO Link Master(UART) and control a small step motor with S7. 

But anyway it is nice to know that you are there !!


Top
  11/29/2012, 1:11 PM
Joined 11/13/2012
Last visit: 2/12/2013
Posts: 8
Rating:
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Hello again,

I have installed the GSD data and found the device in the Hardware Catalog. In order to communicate with TPS-1 i made the network. 

Could you please give me an idea, to at least display something to LCD Display of TSP-1?

Thanks !


Top
  12/2/2012, 6:21 AM
Joined 8/31/2010
Last visit: 1/27/2015
Posts: 1486
Rating:
Rated: Excellent [4.01 out of 5 / rated 154 time(s)]. (154) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
aachener_1 schrieb:
Hello again,

I have installed the GSD data and found the device in the Hardware Catalog. In order to communicate with TPS-1 i made the network. 

Could you please give me an idea, to at least display something to LCD Display of TSP-1?

Thanks !



Hello aachener,
got to look into the manual of that display system only. Share that can have a look on that.

Like it? Rate it!
Top
  1/2/2013, 4:04 PM
Joined 11/13/2012
Last visit: 2/12/2013
Posts: 8
Rating:
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 

Yes I did, but the Problem is, there isn t any manual of LCD. All these function are programmed on V850(microcontroller) on the TPS-1 board.  And also all Protocol (Profinet) functions..

The Question is, after the installing GSD datas of TPS-1 whether TIA V11 supports this device(TPS-1) in the sense of usage of these functions which are written on Microcontroller. If yes, how can I use them in TIA, Otherwise should i configure the TPS-1 or any idea pls ?

Thanks !

Attachment: Neue Bitmap.jpg  (29 Downloads)

Top
  11/25/2013, 9:00 AM
Joined 4/24/2009
Last visit: 1/14/2015
Posts: 2814
Rating:
Rated: Outstanding [3.63 out of 5 / rated 133 time(s)]. (133) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
New question splitted to How I can get the 1200 S7 GSD file (profinet)?

Best regards
O_Moderator
Top
Page 1 of 1 (8 items)
Actions