Technical Forum

SIMATIC Panel

Regarding downloading program to siemens ktp600 Basic Pn HMI

Thread Starter: santosh.hs   Started: 3/10/2012 8:25 AM   Replies: 3

« Previous thread Next thread »
Page 1 of 1 (4 items)
  3/10/2012, 8:25 AM
Joined 3/10/2012
Last visit: 4/17/2012
Posts: 2
Rating:
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Hi All

I am facing a problem, that i was trying to download program to KTP600 Basic PN Hmi, but it is not downloading to HMI from pc...
I have Installed TIA-V11, SP2 in my PC.
First thing i ahve done is i have configured the HMI with one PLC.. and assigned IP Address online HMI, and i have made entered same address in offline HMI also. I also setted same IP address in PLC also. Both PLC & HMI are accesible, in Accesible devices window with respective IP Address.
Then after programming PLC & HMI, i tried to download the program for PLC it was downloaded easily but not for HMI....sad
While compiling the HMI Programming File it will not show any error msgs but while downloading the program, downloading wizard will start but after some time, it shows an msg that downloding process will not possible. and will abort the downloading process showing errors-1, warning-0 but if i click on that error status line it will not open so that i am not able to know what might be the problem.
I also tried in other PC's also but it is not happening.. so pls help me regarding this issue...
Top
  3/12/2012, 4:54 PM
Joined 9/5/2011
Last visit: 10/28/2013
Posts: 3037
Rating:
Rated: Outstanding [3.81 out of 5 / rated 155 time(s)]. (155) 
Users with special expertise supervising conferences
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Hello,

Can you post a screenshot of the error message?
Can you use "Go to" at the error message?


Tweety
Top
  3/14/2012, 7:51 AM
Joined 3/10/2012
Last visit: 4/17/2012
Posts: 2
Rating:
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Hi

I tried go to option also by clicking on that error msg but that was continously disabled, hence this option also didnt work...
I dont have screenshot of that process, but it shows a window displaying that...
Error-Load Failed with error (0800-00012)
Cannot Perform Transfer...
Top
  3/14/2012, 10:59 AM
Joined 9/5/2011
Last visit: 10/28/2013
Posts: 3037
Rating:
Rated: Outstanding [3.81 out of 5 / rated 155 time(s)]. (155) 
Users with special expertise supervising conferences
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Hello,

You can delete the IM folder in your project and then you should compile the project new.

Have you downloading another project to KTP 600 Basic?
It this possible?

You can use a demo project from this link.
Demo projects for HMI Panels at WinCC (TIA Portal) for Basic Panels, Comfort Panels and WinCC Runtime Advanced (TIA Portal)

Can you download this project?

Tweety
Top
Page 1 of 1 (4 items)
Actions