Technical Forum

SINUMERIK CNC automation systems

Sinumerik 820GA3

Thread Starter: vak56   Started: 2/3/2012 3:10 PM   Replies: 4

« Previous thread Next thread »
Page 1 of 1 (5 items)
  2/3/2012, 3:10 PM
Joined 6/29/2011
Last visit: 9/20/2013
Posts: 10
Rating:
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Mr Moderator. I can't find anywhere at site this manual: "Sinumerik 820G,GA3, Operator's Guide". Order 6ZB5410-0HR02-0BA0. There is only 810G_GA3. Can you help me? 
Top
  2/5/2012, 8:05 PM
Joined 1/19/2008
Last visit: 2/1/2015
Posts: 436
Rating:
Rated: Excellent [4.53 out of 5 / rated 19 time(s)]. (19) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Hi,

Apart from the row of user buttons along the bottom of the control which are allocated by the machine tool builder I think you will find the operating manual for the 810G is the same as the 820G

Pee
Top
  2/7/2012, 7:47 AM
Joined 6/29/2011
Last visit: 9/20/2013
Posts: 10
Rating:
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
I quite suppose that operator guides 810 and 820 are similar.
But 820G GA3 (6FC3801-3AC-Z) on grinding machine tool "ASP400S-CNC"  "Bahmuller", likely, has 
Any features. For example: in the basic modes in the menu is not present SETTING DATEN on the display. And to change SETTING BITS, I pass such way:
DIAGNOSE>NC-STATUS>SETTIING DATEN>SETTING DATEN>SETTING BITS. There are features of adjustment of interface V.24. Also it is located not on the panel of the operator. Therefore there is a problem of communication with program PCIN. At all how in 810G.
Top
  2/7/2012, 8:49 AM
Joined 1/19/2008
Last visit: 2/1/2015
Posts: 436
Rating:
Rated: Excellent [4.53 out of 5 / rated 19 time(s)]. (19) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Hi,

 I think your problem may be that the machine tool buider has customised the displays for your machine and so they do not work like the Siemens manual.

Have you got the orginal operator manual ?.
Pee
Top
  2/7/2012, 10:26 AM
Joined 6/29/2011
Last visit: 9/20/2013
Posts: 10
Rating:
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Good afternoon. I thank for a prompt reply. Yes, we have an original short operators manual in German (it I do not own, but I will try to understand by means of the translator). Here there are interface V.24 options. Thanks for the help.
Top
Page 1 of 1 (5 items)
Actions