Technical Forum

SIMATIC WinCC

WinCC 7.0 sp3 download

Thread Starter: gre_m   Started: 1/3/2012 10:45 AM   Replies: 5

« Previous thread Next thread »
Page 1 of 1 (6 items)
  1/3/2012, 10:45 AM
Joined 9/27/2005
Last visit: 7/5/2013
Posts: 948
Rating:
Rated: Above avarage [2.68 out of 5 / rated 37 time(s)]. (37) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Siemens make WinCC 7.0 sp3

http://support.automation.siemens.com/WW/view/en/55987264.

before after of the new service pack for WINCC siemens gave a link to download it. Now that there is no link. Is there a link to this or need to contact the local Siemens office
Top
Thank you for this post from:
  1/3/2012, 10:55 AM
Joined 1/3/2006
Last visit: 1/24/2015
Posts: 680
Rating:
Rated: Outstanding [3.86 out of 5 / rated 43 time(s)]. (43) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
HI
WinCC SP3 cant be downloaded. Its a complete and independent product.
You need to order WinCC SP3.
Top
  1/3/2012, 11:33 AM
Joined 3/21/2006
Last visit: 1/23/2015
Posts: 9931
Rating:
Rated: Outstanding [3.92 out of 5 / rated 1054 time(s)]. (1054) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Or to order upgrade SP3 (includes a new license) in case you have there SP2.
Top
  1/3/2012, 12:13 PM
Joined 10/11/2006
Last visit: 1/19/2015
Posts: 1775
Rating:
Rated: Outstanding [3.42 out of 5 / rated 81 time(s)]. (81) 
Users with special expertise supervising conferences
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Hi,

ordering details see in the above mentioned entry. The update ordering number for WinCC V7.0 SP3 is S79220-B3611-P

SIMATIC WinCC Upgrade / Software Update Service (SUS) 1)
WinCC V7 Update 
· zur Hochrüstung von V7.0 -> V7.0 SP3 (nur DVD)S79220-B3611-P
WinCC V7 Upgrade 
· zur Hochrüstung der RT-Version, V6.2 -> V7.06AV6381-2AA07-0AX3
· zur Hochrüstung der RT-Version, V6.0 -> V7.06AV6381-2AA07-0AX4
· zur Hochrüstung der Client RT-Version, V6.2 -> V7.06AV6381-2BC07-0AX3
· zur Hochrüstung der Client RT-Version, V6.0 -> V7.06AV6381-2BC07-0AX4
· zur Hochrüstung der RC-Version, V6.2 -> V7.06AV6381-2AB07-0AX3
· zur Hochrüstung der RC-Version, V6.0 -> V7.06AV6381-2AB07-0AX4
WinCC Software Update Service (SUS) 2) 4)  
enthält aktuelle Updates/Upgrades für WinCC Basissoftware und Optionen  
· 1 Lizenz6AV6381-1AA00-0AX5
· 3 Lizenzen6AV6381-1AA00-0BX5
· 10 Lizenzen6AV6381-1AA00-0CX5
Top
  1/3/2012, 5:16 PM
Joined 9/27/2005
Last visit: 7/5/2013
Posts: 948
Rating:
Rated: Above avarage [2.68 out of 5 / rated 37 time(s)]. (37) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
I understand that WinCC 7.0 Sp3 - this is a separate product.

I have WinCC 7,0 SP2. So I thought that upgrading to WinCC 7.0 Sp3 may be made by downloading over the Internet (WinCC 7.0 Sp3 has same order number as  WinCC 7.0 Sp2) and license update/upgrade not need



=== Edited by gre_m @ 1/3/2012 5:17 PM [GMT ] ===


Top
  10/29/2012, 11:22 AM
Joined 12/7/2011
Last visit: 1/14/2015
Posts: 58
Rating:
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Dear gre_m,

I have same problem with you. I ordered WinCC SP3 but I get WinCC SP2. The part number is same. Any idea?
Top
Page 1 of 1 (6 items)
Actions