Technical Forum

SIMATIC WinCC

Wincc scada ver 7.0 sp2 with windows 7 ethernet connectivity with siemens plc .

Thread Starter: mrk08230   Started: 12/30/2011 5:10 AM   Replies: 2

« Previous thread Next thread »
Page 1 of 1 (3 items)
  12/30/2011, 5:10 AM
Joined 11/18/2011
Last visit: 9/28/2012
Posts: 3
Rating:
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
hi,
i am trying for wincc scada 7.0 with windows 7 ethernet connectivity with siemens plc.
but i am not able to read the plc tags in wincc scada . i have use siemens plc ( 315 2 pn dp ).
i got the success using MPI .but not using ethernet.
also i got the success using allen bradely plc with wincc scada. i am able to read the ab plc (micrologix 1100 ) tags on ethenet using rslinx opc server.
please help to read siemens plc tags in wincc scada using ethernet.when i am trying this , i have monitor the status of driver connection, which is continuously make & brake ( Ok & disconnected ).for every second.
i also get the success using windows xp . same program of wincc scada is run on windows xp & the ethernet connection found ok & i am able to read the siemens plc tags.
how can do this with WINDOWS 7 .
Please help.
Top
  12/30/2011, 7:39 AM
Joined 3/21/2006
Last visit: 1/30/2015
Posts: 9932
Rating:
Rated: Outstanding [3.92 out of 5 / rated 1054 time(s)]. (1054) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Perhaps some screens shots will clarify your settings there. Basically there doesn't sense if the Windows is XP or 7. If the installed software are compatible each other.
Take a look at WINCC and S7300 via Ethernet. (I don't think you need them but in case...)

best regards,
Hristo Mihalev
Top
  1/2/2012, 10:02 AM
Joined 3/6/2008
Last visit: 1/22/2015
Posts: 128
Rating:
Rated: Excellent [4.13 out of 5 / rated 16 time(s)]. (16) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Hi,
do you install  SIMATIC NET software?

Best regards

Jaromir Hladik

Jaromir Hladik

DEL a.s.
Strojirenska 38
591 01 Zdar nad Sazavou
http:\\www.del.cz
Top
Page 1 of 1 (3 items)
Actions