Technical Forum

SIMATIC Panel

Automation License Manager Connection To MP277

Thread Starter: daleb   Started: 12/11/2011 11:20 PM   Replies: 1

« Previous thread Next thread »
Page 1 of 1 (2 items)
  12/11/2011, 11:20 PM
Joined 12/10/2011
Last visit: 1/16/2012
Posts: 2
Rating:
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Trying to connect and install my Sm@rtAccess license to one of our MP277 panels.  Installing licenses and connecting to our other MP277 panels has not been an issue.  We have one panel which we can ping and confirm network connectivity, but cannot connect to HMI device through the license manager.  In Automation License Manager->Edit->Connect Target System->Connect HMI Device, then setting the connection type to Ethernet and making the Computer Name to the connected IP address.  I am not able to connect to one of our 8 MP 277 panels using this method, I am able to connect to all the other MP panels using this same connection method.  

Error Reported is:
Transfer error: 16842752 (0x1010000) - Connection Error.
Top
  12/12/2011, 2:32 AM
Joined 12/10/2011
Last visit: 1/16/2012
Posts: 2
Rating:
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Figured it out....S7 Transfer setting in the MP277 control panel....

Attachment: 12-11-2011 4-32-03 PM.jpg  (148 Downloads)

Top
Thank you for this post from:
Page 1 of 1 (2 items)
Actions