Technical Forum

SIMATIC Panel

TP 700 comfort panel using windows CE sounds for alarms

Thread Starter: ionut.b   Started: 9/20/2011 4:48 PM   Replies: 6

« Previous thread Next thread »
Page 1 of 1 (7 items)
  9/20/2011, 4:48 PM
Joined 1/17/2007
Last visit: 1/14/2015
Posts: 286
Rating:
Rated: Above avarage [2.5 out of 5 / rated 2 time(s)]. (2) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
How to configure windows CE sounds (HMI control panel - "Volume&Sounds Properties" ) to be used when an alarm is generated?


Thank you.
Top
  9/21/2011, 10:52 AM
Joined 4/29/2010
Last visit: 11/25/2014
Posts: 1557
Rating:
Rated: Outstanding [3.62 out of 5 / rated 151 time(s)]. (151) 
Users with special expertise supervising conferences
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Hello,

do you want to use the sounds from the panel or seperate sounds?

best regards
Top
  9/21/2011, 11:06 AM
Joined 1/17/2007
Last visit: 1/14/2015
Posts: 286
Rating:
Rated: Above avarage [2.5 out of 5 / rated 2 time(s)]. (2) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
I could use one of the sounds already configured in the panel; like "Asterisk".

Thank you.
Top
  9/21/2011, 4:50 PM
Joined 4/29/2010
Last visit: 11/25/2014
Posts: 1557
Rating:
Rated: Outstanding [3.62 out of 5 / rated 151 time(s)]. (151) 
Users with special expertise supervising conferences
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Sure this is possible. You find all the soundfiles at the Windows folder (don`t forget to show the systemfolder "View -> Options").

Then, add a button f. e. and project the function "startprogramm" with the parameters
\Windows\ceplayer.exe
\Windows\xxx.wav

If you click the button the sound will play.
Top
  9/22/2011, 10:03 AM
Joined 1/17/2007
Last visit: 1/14/2015
Posts: 286
Rating:
Rated: Above avarage [2.5 out of 5 / rated 2 time(s)]. (2) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Thank you Sandman for your help.

I have tested this method and there are some points that I would like to improve:

1.the aplication ceplayer.exe is displayed in runtime when the alarm is triggered; I could not make it run in background (should be a setting in windows but I don't know it);

2. when the alarm is acknowledged the player should close (I selected Repeat option in Playback menu).

Best regards.
Top
Thank you for this post from:
  9/23/2011, 10:28 AM
Joined 4/29/2010
Last visit: 11/25/2014
Posts: 1557
Rating:
Rated: Outstanding [3.62 out of 5 / rated 151 time(s)]. (151) 
Users with special expertise supervising conferences
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Thanks for sharing this informationRnf:lblSmileyTooltip_ .
Top
  3/21/2014, 7:32 AM
Joined 8/25/2012
Last visit: 5/19/2014
Posts: 3
Rating:
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
sir

alarm sound is not getting reset with the reset button.
 
and if the alarm is not getting reset den also only single time sound is produced,and with
the selection of repeat option alarm does not gets mute even after the wmp. gets reset.

regards

divya

india
Top
Page 1 of 1 (7 items)
Actions