Technical Forum

SIMATIC S5 / STEP 5

RS232 -TTY interface

Thread Starter: jm1983   Started: 9/9/2011 8:40 PM   Replies: 5

« Previous thread Next thread »
Page 1 of 1 (6 items)
  9/9/2011, 8:40 PM
Joined 12/14/2010
Last visit: 7/4/2014
Posts: 160
Rating:
Rated: Outstanding [3.5 out of 5 / rated 4 time(s)]. (4) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
hello to all

I need to connect a S5-95U to a commercial PC and i don't have the interface to make it,but I have an idea and i want to consult it with you and that you give me your opinions.
I have a bus driver C73451-A347-B202 (and the power pack 6DR2900-8BA ) for to connect several SIPART DRs with interfaces RS232 (conector DB9 in the bus driver), to a PC using communication RS232 or to a CP 524/544B of a S5 using TTY (conector DB25 in the bus driver).
The idea is the following one:
 - I configure the bus driver for the communication with a CP of a S5 through TTY and the communication with the SIPART DRs is with RS232 always, of course.
- Knowing the distribution of pins of each side, I build two connection cables, for to use the connection RS232 of the bus driver (for the SIPART DRs) for the PC port and the connection TTY (for the CP) with for the S5 port(SINEC L1).

what do you say?
Top
  9/10/2011, 1:58 AM
Joined 5/28/2008
Last visit: 1/28/2015
Posts: 3288
Rating:
Rated: Outstanding [3.71 out of 5 / rated 598 time(s)]. (598) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Hello,
You can try to buy an interface cable from Process Informatik company. They have USB - S5 cable and I have tried it and it's easy to use.
Hope this helps.

Ayman Elotaify
MISC Egypt
www.miscegypt.com
Top
  9/13/2011, 2:31 PM
Joined 1/11/2011
Last visit: 12/1/2014
Posts: 374
Rating:
Rated: Excellent [4.08 out of 5 / rated 51 time(s)]. (51) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Hello jm1983,

If you use a PC with serial RS232 interface you can take the PC converter cable with the order number 6ES5734-1BD20.
The interface assignment of the PC converter cable finds you here:
http://support.automation.siemens.com/WW/view/en/13063839

Here a further recommendation. I think this solution is better.
Köster-Box (PC-S5-Interface)

Interface for programming Siemens S5-PLCs with the PC.
The Kösterbox converts the RS232 signals of the PC into TTY signals (20mA) of the automation system.

• The box is full duplex, send- and recieve channel,
• the box is active for programming S5 90-115U,
• for S5-135/155U and CP or acting passively with other cable,
• the box has its own power supply with galvanic separation

Her the link:
http://www.koester-systemtechnik.de/Koester_Box_E.html

Best regards
Azteke0110

Top
  9/13/2011, 6:57 PM
Joined 12/14/2010
Last visit: 7/4/2014
Posts: 160
Rating:
Rated: Outstanding [3.5 out of 5 / rated 4 time(s)]. (4) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Thanks a lot for your answers.
I don't have the money to buy an interface, therefore I need to make one. Can you help me in this?.

Thanks in advanced.
Top
  9/13/2011, 9:52 PM
Joined 3/21/2006
Last visit: 1/27/2015
Posts: 9931
Rating:
Rated: Outstanding [3.92 out of 5 / rated 1054 time(s)]. (1054) 
Users with special expertise supervising conferences
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Hello,

Take a look there S5 programming cable 

Best regards,
Hristo Mihalev
Top
  9/14/2011, 2:20 PM
Joined 12/14/2010
Last visit: 7/4/2014
Posts: 160
Rating:
Rated: Outstanding [3.5 out of 5 / rated 4 time(s)]. (4) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Thank you very much for your help UMENCHO.
Top
Page 1 of 1 (6 items)
Actions