Technical Forum

Communication / Networks

Profinet to Profibus Conversion

Thread Starter: ssmanku1699   Started: 9/3/2011 1:16 PM   Replies: 2

« Previous thread Next thread »
Page 1 of 1 (3 items)
  9/3/2011, 1:16 PM
Joined 8/10/2009
Last visit: 12/1/2014
Posts: 129
Rating:
Rated: Good [1 out of 5 / rated 1 time(s)]. (1) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 

Dear Users,

I am having one CPU 313C2 DP  and I need to  integrate the same on profinet . So I need  a way of  communicating the same plc of DP port with  a profinet port in another system. I think for that I need a Profibus to Profinet converter. Please Suggest. Is there any CP for the same which can be integrated along with CPU 313C2DP ?

 

Thanks.

Your's Truly,

Sarabjot Singh Manku

Top
  9/3/2011, 1:58 PM
Joined 10/7/2005
Last visit: 1/26/2015
Posts: 2605
Rating:
Rated: Excellent [4.3 out of 5 / rated 736 time(s)]. (736) 
Users with special expertise supervising conferences
Rated: Excellent [5 out of 5 / rated 1 time(s)]. (1) 
Hello ssmanku1699

you have a few options to achive your goal:

1.) Assuming your 313C's DP port is NOT needed as a DP Master, you configure it for DP Slave mode and add an IE/PB Link to it as the Gateway to the Profinet I/O Controller.

2.) Add a CP343-1 to the 313C system and configure it as a Profinet I/O device.

3.) If your 313C's DP port is used as a DP Master port, you could still go with option 1 but will need to add a DP/DP coupler additionally (least favourite option to be honest, purely mentioned for completeness).

And here are a few selected example links with more on the above:
Where do you find sample programs and documentation on communication between S7-400 (PROFINET IO controller) and S7-300 (I slave) incorporating an IE-to-PB link gateway? 
Where can you find information on the topic of PROFINET?
How do you program communication blocks FC11 and FC12 for the PROFINET IO device?

I hope this helps    

Cheers

fritz

The advice and opinion given in this thread is that of the author and does not necessarily reflect the views of I S Systems Pty Limited.
To find out how I S Systems can help you with your automation needs please visit www.issystems.com.au.
Top
Thank you for this post from:
  9/30/2014, 2:05 PM
Joined 9/3/2014
Last visit: 1/26/2015
Posts: 705
Rating:
Rated: Outstanding [4 out of 5 / rated 9 time(s)]. (9) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 


New question published by MBS is split to a separate thread with the subject Profinet to Profibus Conversion CPU is 317-2DP and HMI KTP1000 Basic .


Best regards
Min_Moderator




=== Edited by Min_Moderator @ 9/30/2014 3:40 PM [GMT ] ===


Top
Page 1 of 1 (3 items)
Actions