Technical Forum

Visualization general

Differences between WinCC and WinCC flexible

Thread Starter: ignacio85   Started: 11/24/2010 2:38 PM   Replies: 6

« Previous thread Next thread »
Page 1 of 1 (7 items)
  11/24/2010, 2:38 PM
Joined 2/17/2010
Last visit: 2/16/2011
Posts: 19
Rating:
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
I have one question about WinCC, We are thinking about developping an application that will run in a PC to make the supervision of a production line and to other fonctionalities. We are looking which software is better to develop it. I've been reading about WinCC and it seems a really powerful tool. I'm trying to compare if It would be enough for us to develop our application with WinCC felixible and install it like a RT in the PC.
Which are the main differences? Do WinCC applications allow to run more than one script at the same time?
Does WinCC flexible running as RT allow it? Because for one past project we were working with WinCC flexible on a MP377 and one of the biggest problem was that we needed to wait that one script was finish to make another one start.

Regards,
Ignacio
Splitted from WinCC supervisor cost.



=== Edited by O_Moderator @ 11/25/2010 8:05 AM [GMT ] ===
new subject after splitting

Top
  12/9/2010, 7:24 PM
Joined 6/29/2010
Last visit: 1/26/2015
Posts: 112
Rating:
Rated: Excellent [4.56 out of 5 / rated 48 time(s)]. (48) 
Rated: Excellent [4.33 out of 5 / rated 3 time(s)]. (3) 
Hi ignacio85,

Follows a description of these options:

 

 WinCC WinCC flexible RT
Different Architectures Yes No (only single station)

 

Maximum number of Tags 262144 4096

 

Backup (alarms + trends) Yes No *1

 

Popup window Yes Yes, but too limited.

 

Integrated Database SQL Server CSV or RDB

 

Scripts Yes (“C” and VB) VB, limited to 200.

 

Animation of complex objects Yes (size, rotation, etc.) No

 

RecipesOptional Optional

 

RedundancyOptional No

 

Historical Trends Up to 512 or + Up to 100 (with licence Optional)

 

Web AccessYes (Optional) Yes, with limitations (Optional)

 

Use of more than one monitor Yes No

 

Screen resolution any only pre-defined

 

Price X < X

 

  *1 It is possible to program it by the way scripts, but with limitations.

Regards.



=== Edited by MrPaiva @ 1/20/2011 1:22 PM [GMT ] ===


=== Edited by MrPaiva @ 12/17/2010 5:25 PM [GMT ] ===


=== Edited by MrPaiva @ 12/10/2010 1:05 PM [GMT ] ===


=== Edited by MrPaiva @ 12/10/2010 1:04 PM [GMT ] ===


Top
Thank you for this post from:
  12/14/2010, 10:10 AM
Joined 12/10/2010
Last visit: 5/2/2012
Posts: 37
Rating:
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
WINCC is a scada program like INTOUCH
WINCC flexible was created to programm HMI, it s not a SCADA program



=== Edited by seb_nancy @ 12/14/2010 10:11 AM [GMT ] ===


Top
  1/29/2011, 9:23 AM
Joined 5/14/2009
Last visit: 11/22/2013
Posts: 151
Rating:
Rated: Excellent [4.5 out of 5 / rated 2 time(s)]. (2) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
hi
friends you forgot a clear difference.

wincc flexible commonly used for configuring hmi panels.
but wincc don't support this part.

clearly simatic wincc is better than wincc flexible for scada and pc based monitoring.

good luck
Top
  2/9/2011, 12:50 PM
Joined 6/29/2010
Last visit: 1/26/2015
Posts: 112
Rating:
Rated: Excellent [4.56 out of 5 / rated 48 time(s)]. (48) 
Rated: Outstanding [4 out of 5 / rated 1 time(s)]. (1) 
Hi bermuda,

You're right, but the comparation is between WinCC and Wincc flexible RT (running at PC).

Only for reinforce, WinCC is a SCADA system and Wincc flexible is a software for programming panels.
Top
  2/10/2011, 3:54 PM
Joined 4/19/2006
Last visit: 4/17/2014
Posts: 1275
Rating:
Rated: Outstanding [4 out of 5 / rated 114 time(s)]. (114) 
Rated: Outstanding [4 out of 5 / rated 1 time(s)]. (1) 
  Hello,

  WinCC Flexible can be used for a smaller stand-alone SCADA system, with limited functionallities. It can monitor variables, you can have screens and scripts. However the data export and connectivity options are definitely not like WinCC. It also has less options and can handle few tags.
  If you need scripts, extensive reporting or connectivity go with WinCC!
  Best regards,

  Danielle

Danielle Crespo Cavalcanti

Simatec Tecnologia em Automação
Belo Horizonte - MG - Brazil
www.simatec.com.br
Top
Thank you for this post from:
  8/24/2011, 6:38 PM
Joined 1/15/2011
Last visit: 5/28/2012
Posts: 3
Rating:
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Many thanks!laugh
Top
Page 1 of 1 (7 items)
Actions