Technical Forum

SIMATIC WinCC (TIA Portal)

MSI File initialization failed-Error Install remote prohibited

Thread Starter: luciferC4   Started: 8/10/2011 7:48 PM   Replies: 8

Tags TIA WinCC Installation Options General

« Previous thread Next thread »
Page 1 of 1 (9 items)
  8/10/2011, 7:48 PM
Joined 1/25/2006
Last visit: 1/25/2015
Posts: 239
Rating:
Rated: Excellent [4.39 out of 5 / rated 18 time(s)]. (18) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Hi,today I bought Wincc V11 professional I tried to install software. But in step Configuration appeared message as in subject of this post. I have windows 7 64-bit with virtual XP OS where I tried to install.
Can someone tell me what's wrong.
Thanks.
Top
  8/10/2011, 9:56 PM
Joined 7/24/2008
Last visit: 1/30/2015
Posts: 2580
Rating:
Rated: Excellent [4.35 out of 5 / rated 461 time(s)]. (461) 
Users with special expertise supervising conferences
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Hi,

That I know, the TIA will be released for Windows 64 bits just from V11 SP2 (not yet avaliable sad). At other side, there is no offitial garanty that it runs in virtual machines.
Witch XP version do you have (XP SP3)?
Can you post the printscreen of the error message?



=== Edited by Pegaia @ 8/10/2011 9:59 PM [GMT ] ===


=== Edited by Pegaia @ 8/10/2011 9:58 PM [GMT ] ===



Denilson Pegaia
Siemens Industry Sector
- Technical Support & Hotline -
Hotline – Atenção ao Cliente / Customer Care
Tel.: +55 11 3833-4040
E-Mail: atencao.cliente.ac.br@siemens.com
Top
  8/11/2011, 8:14 AM
Joined 1/25/2006
Last visit: 1/25/2015
Posts: 239
Rating:
Rated: Excellent [4.39 out of 5 / rated 18 time(s)]. (18) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Hi,
here, you can see screenshot whit error. About Xp, that is XP SP3.

Attachment: screen.JPG  (181 Downloads)

Top
  8/11/2011, 9:13 AM
Joined 10/19/2005
Last visit: 1/30/2015
Posts: 1518
Rating:
Rated: Outstanding [3.72 out of 5 / rated 104 time(s)]. (104) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Hi,

i mean too. the problem are your PC System

Look to this links
-> http://support.automation.siemens.com/WW/view/en/51120883 
-> http://support.automation.siemens.com/WW/view/en/49740133 

There are described which Systen you can use.

regards,
Top
  8/11/2011, 11:25 AM
Joined 1/25/2006
Last visit: 1/25/2015
Posts: 239
Rating:
Rated: Excellent [4.39 out of 5 / rated 18 time(s)]. (18) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Exactly, that is XP professional SP3, 32-bit. This OS is installed on virtual machine under windows 7 professional 64-bit as compatibility XP mode. Under XP, I installed all Siemens and other 32-bit software (step 7, microwin, TIA portal 10.5, wincc flexible 2008, logosoft,....) and all work properly...
BR
Top
  8/11/2011, 10:40 PM
Joined 5/19/2006
Last visit: 1/9/2015
Posts: 531
Rating:
Rated: Excellent [4.32 out of 5 / rated 81 time(s)]. (81) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Can you attach (zip) here the .log files from "C:\Documents and Settings\All Users\Application Data\Siemens\Automation\Logfiles\Setup\"

Dec
Top
  8/14/2011, 8:41 AM
Joined 1/25/2006
Last visit: 1/25/2015
Posts: 239
Rating:
Rated: Excellent [4.39 out of 5 / rated 18 time(s)]. (18) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 

this is logfile for Wincc V11. If you need all files (there are many), I'll send you.
BR.


Attachment: SIA_WINCC_PROFESSIONAL_V11.zip  (97 Downloads)

Top
  8/15/2011, 4:32 PM
Joined 5/19/2006
Last visit: 1/9/2015
Posts: 531
Rating:
Rated: Excellent [4.32 out of 5 / rated 81 time(s)]. (81) 
Rated: Excellent [5 out of 5 / rated 1 time(s)]. (1) 

Looking at your log file I see:
08:04:27|WARNING   |MsiSetupPlus::CustomInitialize()        |(07) Error Opening MSI Package. ERROR_INSTALL_REMOTE_PROHIBITED; Details: ; Path: \\TSCLIENT\E\InstData\UCLES\Media\WINCCBASUCL.msi

Now I am not sure as why this error occurs but we can clarify very quickly:
1. Do you connect via remote desktop on that virtual machine? If yes, can you open the VM console screen and try to install again.
2. If the above is not true can you copy all the setup files locally on your vm folders (C:\SetupDirTmp\) and run the setup again?

Dec

Top
Thank you for this post from:
  8/16/2011, 3:21 PM
Joined 1/25/2006
Last visit: 1/25/2015
Posts: 239
Rating:
Rated: Excellent [4.39 out of 5 / rated 18 time(s)]. (18) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Hello Dec,
I accepted your second advice and copy all DVD on c root of local disk. After that, software was installed without problem. Thank you very much.
Top
Page 1 of 1 (9 items)
Actions