Technical Forum

LOGO!

LOGO!SoftComfort V7

Thread Starter: moss   Started: 7/22/2011 12:28 PM   Replies: 11

« Previous thread Next thread »
12» Page 1 of 2 (12 items)
  7/22/2011, 12:28 PM
Joined 9/13/2007
Last visit: 8/19/2013
Posts: 8
Rating:
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Why upgrade proposed by the Update Center intall an older version of the current 6.1.12 ?
Top
  7/22/2011, 12:34 PM
Joined 12/27/2006
Last visit: 2/1/2015
Posts: 648
Rating:
Rated: Outstanding [3.8 out of 5 / rated 44 time(s)]. (44) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
I think.....
you doing someting wrong.
In LOGO!Comfort V6.. yup go to the HELP menu, and update via internet.
Then you get LOGO! Comfort V7.0.30
Top
  7/22/2011, 1:07 PM
Joined 9/13/2007
Last visit: 8/19/2013
Posts: 8
Rating:
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
I just ran the update process, but on the Italian language continues to install an old version of V6.
Top
  7/22/2011, 1:29 PM
Joined 3/21/2006
Last visit: 1/30/2015
Posts: 9932
Rating:
Rated: Outstanding [3.92 out of 5 / rated 1054 time(s)]. (1054) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
If I am not wrong there is a difference between UPGRADE and UPDATE options...blush

Best regards,
Hristo Mihalev
Top
  7/23/2011, 12:07 AM
Joined 4/22/2010
Last visit: 2/1/2015
Posts: 5524
Rating:
Rated: Excellent [4.3 out of 5 / rated 583 time(s)]. (583) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
The update/ upgrade is not working o.k. now.

Perhaps to mutch traffic.

I have one system o.k. now with v7 but other system, no sign of update/ upgrade.

Think patience is the keyword.

And if you get the v7 software, Be happygringrin

Looks good.

Regards,

Marcjan

Problem solved?
Please let us know!

Please no technical questions by PM, use the forum sections for your questions.
Top
  7/25/2011, 8:14 AM
Joined 7/24/2006
Last visit: 1/29/2015
Posts: 2267
Rating:
Rated: Outstanding [3.79 out of 5 / rated 289 time(s)]. (289) 
Users with special expertise supervising conferences
Rated: Excellent [5 out of 5 / rated 1 time(s)]. (1) 
Hi,

to update to LSC V7 you need LSC V6.1.

If you have LSC V6.0, than you need to update to V6.1 first.

Differents update upgrade:
Update is a x.luf file. Only LSC and the online help will be updated. Actually only possible via LSC Help/Update Center.

Upgrade is the same then the LOGO! Soft Comfort Upgrade DVD.
Here everything will be installed. Inluding the new Manuals, CAD-Darwings, .....

Hope this helps
Top
Thank you for this post from:
  7/28/2011, 2:59 PM
Joined 6/24/2010
Last visit: 1/31/2015
Posts: 21
Rating:
Rated: Outstanding [4 out of 5 / rated 1 time(s)]. (1) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Am I right in thinking this only supports 32 bit Windows 7 at the moment. I have tried to update from the help menu, the file downloads ok but after clicking next it comes up with an error - java io exception - access denied?!
Top
  7/29/2011, 1:12 AM
Joined 3/26/2009
Last visit: 1/12/2015
Posts: 40
Rating:
Rated: Excellent [4.7 out of 5 / rated 10 time(s)]. (10) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
donkey,
run the version 6 in a compatible mode of windows xp in your windows 7 machine. i did that and the update worked great , i have a 64bit windows 7 machine.

derf
Top
Thank you for this post from:
  7/29/2011, 7:42 AM
Joined 6/24/2010
Last visit: 1/31/2015
Posts: 21
Rating:
Rated: Outstanding [4 out of 5 / rated 1 time(s)]. (1) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Hi Fred,

I have got V6.12 running fine normally under win7 64bit even though it's not officially supported.
But when opening V6.12 in compatabilty mode and doing the update from there it does install. It also then seems to run fine back in normal Win 7 64 bit mode after the update.

Thanks for the advise

Richard
Top
  7/30/2011, 8:08 PM
Joined 9/17/2009
Last visit: 11/13/2013
Posts: 2
Rating:
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 

Visit...

http://logicaycontrol.blogspot.com/2011/07/nueva-version-logosoft-v70-ya.html

best regards
Top
12» Page 1 of 2 (12 items)
Actions