Technical Forum

STEP 7 / STEP 7 Lite

SIMATIC Manager V5.5

Thread Starter: Mushriq   Started: 5/22/2011 9:51 AM   Replies: 16

« Previous thread Next thread »
12» Page 1 of 2 (17 items)
  5/22/2011, 9:51 AM
Joined 8/8/2009
Last visit: 5/1/2013
Posts: 12
Rating:
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
I had installed SIMATIC Manger V5.5 on my Winows 7 OS laptop, I had problem after creating projects i cannot edit OB1 ,the pan opens ,but the program halts with following message (S7-programme has stopped working) ,other things in main window are working Ok.
Top
  5/22/2011, 10:27 AM
Joined 3/21/2006
Last visit: 1/27/2015
Posts: 9931
Rating:
Rated: Outstanding [3.92 out of 5 / rated 1054 time(s)]. (1054) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Hello,

Could be a compatibility problem between Windows7 and Step7. If the OS there is 32bits then reinstall of Step7 might helps.

Best regards,
Hristo Mihalev
Top
  5/23/2011, 2:54 PM
Joined 4/13/2011
Last visit: 2/16/2012
Posts: 11
Rating:
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Hi, may be you have virus and it stopped one of the services in windows. regards Abdul
Top
  5/23/2011, 3:42 PM
Joined 3/15/2008
Last visit: 1/27/2015
Posts: 6727
Rating:
Rated: Excellent [4.03 out of 5 / rated 691 time(s)]. (691) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Mushriq wrote:
...Winows 7 OS...


Do you have Win7 ultimate or professional,  32 Bit?

Industrieautomation: Softwareerstellung und Inbetriebnahme weltweit.
http://www.ibn-service.com
Top
  5/23/2011, 4:08 PM
Joined 11/15/2006
Last visit: 1/13/2015
Posts: 1278
Rating:
Rated: Excellent [4.02 out of 5 / rated 137 time(s)]. (137) 
Users with special expertise supervising conferences
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Is it a tablet PC? Do you have 5.5 with latest HF5 or without?
Please give some more details, otherwise we are not able to give you some help.

Have Fun!

TomDeWou
Top
  5/23/2011, 4:20 PM
Joined 3/21/2006
Last visit: 1/27/2015
Posts: 9931
Rating:
Rated: Outstanding [3.92 out of 5 / rated 1054 time(s)]. (1054) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
TomDeWou wrote:
...Do you have 5.5 with latest HF5 or without?
...

OFFTOPIC
Did you mean Step7 5.5 HF5? As I know the last is number 3. Could give us more details?

Best regards,
Hristo Mihalev
Top
  5/23/2011, 10:08 PM
Joined 9/27/2005
Last visit: 7/5/2013
Posts: 948
Rating:
Rated: Above avarage [2.68 out of 5 / rated 37 time(s)]. (37) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
may be insufficient access rights? In Windows 7 system file protection extended over Windows XP
Top
  5/24/2011, 7:45 AM
Joined 9/6/2008
Last visit: 1/27/2015
Posts: 1076
Rating:
Rated: Outstanding [3.87 out of 5 / rated 61 time(s)]. (61) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 

 Hi Mushriq

Well did you install any microsoft updates, because some updates are not recaommended by Siemens.

Please check if you have anti virus on auto protect or any firewall. Because once i had installed Kaspersky and had lot of problems with Step7 V 5.4

Have fun..Rnf:lblSmileyTooltip_

TAGOLOVER
Top
  5/24/2011, 6:26 PM
Joined 9/27/2005
Last visit: 7/5/2013
Posts: 948
Rating:
Rated: Above avarage [2.68 out of 5 / rated 37 time(s)]. (37) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Hi  Tagolover



I will never install an antivirus on my work computer. Virus protection and security should be implemented organizational methods. Viruses themselves do not appeargrin. If you installed Kaspersky -  add to trusted programs  Step7 - will be less problems. Kaspersky previously reported and the virus in Setup Step7 V 5.5.grin

Top
  5/25/2011, 11:28 AM
Joined 8/8/2009
Last visit: 5/1/2013
Posts: 12
Rating:
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 

I have Win7 ultimate
Top
12» Page 1 of 2 (17 items)
Actions