Technical Forum

STEP 7 Additional Software

USB PC Adapter not working with Step7 V5.5

Thread Starter: josemiall   Started: 5/19/2011 4:40 PM   Replies: 8

« Previous thread Next thread »
Page 1 of 1 (9 items)
  5/19/2011, 4:40 PM
Joined 4/15/2011
Last visit: 8/6/2012
Posts: 12
Rating:
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 

Hello!

I installed Step 7 v5.5 on my Windows 7 several weeks ago and I haven't been able yet to connect online to PLCs with the usb pc adapter. 

The problem is that when I try to select the USB conection in the "Local Connection" tab of the PG/PC selection window, it only appears the COM1 option.

I have read in the forum that the Step 7 v5.5 has implemented de usb drivers for the PG/PC but how can I select it?? Do I need to activate it or do something special??

Many thanks in advance!!

I attach the view of the local connection options of the PG/PC window (sorry it is in spanish blush)

Attachment: PG_PC_no_USB.jpg  (522 Downloads)

Top
  5/19/2011, 5:22 PM
Joined 5/28/2008
Last visit: 1/28/2015
Posts: 3288
Rating:
Rated: Outstanding [3.71 out of 5 / rated 598 time(s)]. (598) 
Rated: Good [1 out of 5 / rated 1 time(s)]. (1) 
Hello,
Although Step 7 V5.5 is compatible with Windows 7 as per mentioned in the following link:

But it is not clearly mentioned that the USB PC adapter is compatible with Windows 7.
Check Page 13 of this manual
Hope this helps.

Ayman Elotaify
MISC Egypt
www.miscegypt.com
Top
  5/19/2011, 5:28 PM
Joined 3/21/2006
Last visit: 1/30/2015
Posts: 9932
Rating:
Rated: Outstanding [3.92 out of 5 / rated 1054 time(s)]. (1054) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Hello,

There is need it only to select the PC Adapter (Auto) and the other setting you could leave them by default. Frankly speaking I am using this kind of adapter but never checked what I have in options. If you a;lready tried and isn't working, perhaps reinstall of Step7 will solve the problem.

Best regards,
Hristo Mihalev
Top
  5/19/2011, 11:29 PM
Joined 10/12/2006
Last visit: 1/31/2015
Posts: 207
Rating:
Rated: Outstanding [4 out of 5 / rated 17 time(s)]. (17) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Hi,

if it's a first install, you need a PLC, because the PC adapter need 24V, from there.
So
1. plug adapter to usb,
2. plug adapter to PLC
3. install the driver from CD

after then you can select the USB.

Regards Zenta



=== Edited by Zenta @ 5/19/2011 11:38 PM [GMT ] ===


Top
  5/21/2011, 10:55 AM
Joined 9/27/2005
Last visit: 7/5/2013
Posts: 948
Rating:
Rated: Above avarage [2.68 out of 5 / rated 37 time(s)]. (37) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Hello josemiall

May be should update firmware and driver for adapter.


For Windows 7 you must use the drivers from the SIMATIC Device Drivers. The driver on the CD USB Prommer 10/2007 / PC Adapter USB 10/2007 is not released for Windows 7.


see   Installation of the PC Adapter USB/USB Prommer Driver with STEP7 V5.5 http://support.automation.siemens.com/WW/view/en/44914284

Have you tried reinstalling the drivers for PC adapter USB indicate search the driver on the installation disk Step7, in the folder where you installed STEP7. May be step7 5.5 include new driver?

as variant - install XP-mode and SIMATIC PC Adapter USB Software V2.0. My colleagues argue that it works



=== Edited by gre_m @ 5/21/2011 2:03 PM [GMT ] ===


=== Edited by gre_m @ 5/21/2011 11:13 AM [GMT ] ===


Top
  5/24/2011, 9:39 AM
Joined 4/15/2011
Last visit: 8/6/2012
Posts: 12
Rating:
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Hello,

First of all thanks for your answers!!

I didn't find the solution yet but I will continue with some tests and I'll let you know. 

Thanks again for your help.
Top
  11/14/2012, 3:58 AM
Joined 9/21/2010
Last visit: 1/27/2015
Posts: 12
Rating:
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Please follow this.
1.In Step7 V5.5 ,No need to install driver(V2.0)
2.Plug every thing to MPI (Need- 24 Vdc. supply to Pc adaptor),USB
3.At pg/pc Select PC adaptor (Auto).
4.Is ok.
Top
  8/6/2014, 11:00 PM
Joined 5/12/2011
Last visit: 8/6/2014
Posts: 1
Rating:
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 

If you just installed Step7 manager, then just plug the adaptor to PLC and to your computer, the USB will appear automatically in the list of local connections if you don't have PLC you can connect 24vdc to the addaptor directly using the adaptor pin assignment sheet in this manual:
https://support.automation.siemens.com/WW/llisapi.dll?func=cslib.csinfo&lang=en&objid=16983464&caller=view

Top
  11/28/2014, 9:54 AM
Joined 2/16/2013
Last visit: 11/28/2014
Posts: 2
Rating:
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Hi.
this situation happened to me and finally i found that my pc adapter usb is fake maybe from china and i put an original one and it recognized by win7 without any problem.
Top
Page 1 of 1 (9 items)
Actions