Technical Forum

MICROMASTER

Midimaster ECO

Thread Starter: bolboreta   Started: 3/1/2011 5:42 PM   Replies: 2

« Previous thread Next thread »
Page 1 of 1 (3 items)
  3/1/2011, 5:42 PM
Joined 12/21/2009
Last visit: 12/26/2014
Posts: 4
Rating:
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Hello,
I've an relatively old MIDIMASTER ECO and I'd like to reverse the rotation of the motor with the digital inputs. I don't know if it is possible in this kind of inverter; In the MM440 it's really, really easy.
I need your help. Thanks in advance.
Top
  3/2/2011, 11:13 PM
Joined 6/4/2008
Last visit: 1/24/2015
Posts: 988
Rating:
Rated: Excellent [4.41 out of 5 / rated 242 time(s)]. (242) 
Users with special expertise supervising conferences
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Hi, as per the attached Midi Eco manual, it does not appear to be possible (unbelievably) to do this with parameters and Digital inputs. You can't even set a negative Fixed frequency as they appear to be clamped between 0 and 150Hz.

I am assuming that you can't set P51 - P56 to a 2 (On Left) or a 3 (Reverse) as you could with the older Midimasters???

Regards,
Graeme

Attachment: MME OperatingInst B.pdf  (5 Downloads)

There are 10 types of people . . .
Those who understand Binary, and those who don't.

Top
  3/10/2011, 7:41 PM
Joined 12/21/2009
Last visit: 12/26/2014
Posts: 4
Rating:
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Yes, unbelievably it's impossible  to set P51 - P56 to a 2 (On Left) or a 3 (Reverse), possibly because the Midimaster ECO was designed for use with pumps and fans.
Regards,
Bolboreta.
Top
Page 1 of 1 (3 items)
Actions