Technical Forum

Communication / Networks

GSD File for DP/AS Interface - 6GK1 415–2AA10

Thread Starter: Navnag   Started: 12/9/2010 6:56 AM   Replies: 7

« Previous thread Next thread »
Page 1 of 1 (8 items)
  12/9/2010, 6:56 AM
Joined 11/21/2007
Last visit: 1/30/2015
Posts: 1614
Rating:
Rated: Excellent [4.1 out of 5 / rated 136 time(s)]. (136) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Hello

Where can I download the Hardware update / GSD file for DP/AS interface module : 6GK1 415–2AA10.

I am not able to locate the same in STEP7 hardware list even after performing a hardware update.

Also the link in the manual of the unit :


http://support.automation.siemens.com/WW/view/en/113250

provides GSD files of version of 6GK1 415-2AA01 only.
Although I am able to communicate with the module using the device definition of -2AA01 module, I do do not know if it leads to any incompatibilities.

Thanks
Navnag


There is no such thing as the last bug in a program
There are no stubborn bugs, There are only stubborn Debuggers.
Top
  12/9/2010, 7:38 AM
Joined 3/21/2006
Last visit: 1/30/2015
Posts: 9932
Rating:
Rated: Outstanding [3.92 out of 5 / rated 1054 time(s)]. (1054) 
Users with special expertise supervising conferences
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Hello,

Which version of Step7 do you have? Try to import HW catalog from attachment.

Best regards,
Hristo Mihalev

Attachment: DPAsi.zip  (131 Downloads)

Top
  12/9/2010, 9:17 AM
Joined 11/21/2007
Last visit: 1/30/2015
Posts: 1614
Rating:
Rated: Excellent [4.1 out of 5 / rated 136 time(s)]. (136) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Thanks Umencho

I am using V5.4 + SP4.

The Attachment you have sent is a .DAT file. how do I import it in Hardware Catalog ?

Regards

Navnag

There is no such thing as the last bug in a program
There are no stubborn bugs, There are only stubborn Debuggers.
Top
  12/9/2010, 9:28 AM
Joined 3/21/2006
Last visit: 1/30/2015
Posts: 9932
Rating:
Rated: Outstanding [3.92 out of 5 / rated 1054 time(s)]. (1054) 
Users with special expertise supervising conferences
Rated: Outstanding [4 out of 5 / rated 1 time(s)]. (1) 
Open hardware configuration->Option->Edit Catalog Profile. Then profile->Import...
Update Step7 5.4 to SP5.( Service Pack 5 for STEP 7 V5.4 and STEP 7 Professional Edition 2006).

Best regards,
Hristo Mihalev
Top
  12/10/2010, 5:21 PM
Joined 2/14/2006
Last visit: 10/16/2014
Posts: 5820
Rating:
Rated: Outstanding [3.96 out of 5 / rated 370 time(s)]. (370) 
Users with special expertise supervising conferences
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Dear Navnag,

if you read the delivery release of the Gateway:
 
Delivery release: DP/AS-Interface Link 20E acc. to AS-i V3.0 (6GK1 415-2AA10)

you will find the following information:

In STEP 7 HWConfig via the hardware catalog entry "DP/AS-i Link 20E Product Version 3" or in third-party systems via the GSD files for 6GK1415 2AA01. (The fourth output of an A/B slave with 4DI/4DO can only be addressed via the GSD file under STEP7 V5.4 SP4.)

Best regards
J_Bell
Top
Thank you for this post from:
  2/2/2011, 11:52 AM
Joined 1/18/2011
Last visit: 9/30/2014
Posts: 39
Rating:
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Hi

Thanks a lot guys even i was searching for that gsd file ,and finally i got it

You r doing great job,,keep it up 

grin 

Rnf:lblSmileyTooltip_
Top
Thank you for this post from:
  4/20/2011, 8:22 AM
Joined 7/13/2009
Last visit: 3/13/2014
Posts: 2
Rating:
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 

Dear zakir,

please send me the GSD file for DP/AS-i link 20E(6GK1 415-2AA10)?

Regards,

Vikram

Top
  4/20/2011, 8:32 AM
Joined 7/13/2009
Last visit: 3/13/2014
Posts: 2
Rating:
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
dear Umencho,

we could import the dat file. But the 6GK1 415-2AA10 is appearing as a folder in HW catalog. Hence we are not able to insert it in a configuration. Please see the screenshot attached.
Kindly suggest a remedy.

regards,
Vikram

Attachment: DP AS-i link catalog.JPG  (76 Downloads)

Top
Page 1 of 1 (8 items)
Actions