Technical Forum

Communication / Networks

maximum distance of profibus cable

Thread Starter: R&R   Started: 1/27/2011 10:35 PM   Replies: 4

« Previous thread Next thread »
Page 1 of 1 (5 items)
  1/27/2011, 10:35 PM
Joined 10/20/2009
Last visit: 1/6/2015
Posts: 69
Rating:
Rated: Outstanding [4 out of 5 / rated 1 time(s)]. (1) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Dear Experts,
                   1.Iam using RIO panels for two areas maximum distance from main panel to one area is                         110mtrs,from that first RIO panel to next RIO panel is 200mtrs .
                   2.Is it possible will communicate through profibus without using any repeaters.It is                                 redundunt IM.
RGDS,
R.R

R&R
LEARN something today so you can TEACH something tomorrow.
DETAIL in your question promotes DETAIL in my answer.
Top
  1/28/2011, 8:13 AM
Joined 3/21/2006
Last visit: 1/23/2015
Posts: 9931
Rating:
Rated: Outstanding [3.92 out of 5 / rated 1054 time(s)]. (1054) 
Users with special expertise supervising conferences
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Hello,

Look there Acceptable line length in PROFIBUS-DP networks

Best regards,
Hristo Mihalev
Top
Thank you for this post from:
  3/10/2012, 8:41 AM
Joined 3/20/2011
Last visit: 11/10/2013
Posts: 5
Rating:
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
are that in the literature
Acceptable line length in PROFIBUS-DP networks
 is the transfer rate relationship with the total of profibus line length or with the node to node profibus line length ?
Top
  3/10/2012, 9:44 AM
Joined 1/28/2009
Last visit: 1/26/2015
Posts: 5090
Rating:
Rated: Excellent [4.25 out of 5 / rated 790 time(s)]. (790) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
stevanus wrote:
are that in the literature
Acceptable line length in PROFIBUS-DP networks
 is the transfer rate relationship with the total of profibus line length or with the node to node profibus line length ?


Dear  stevanus,
Total length for a PROFIBUS segment is listed there.A segment
can be built up from a maximum 32 stations and 2-segments can
be connected with repeaters such as:



Best regards,
Hamid Hosseini
Top
  3/10/2012, 10:53 AM
Joined 3/20/2011
Last visit: 11/10/2013
Posts: 5
Rating:
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Dear Expert,

thanks for all the help, now i understand how to connect the bus correctly laugh

Best Regards,


   Stevanus
Top
Thank you for this post from:
Page 1 of 1 (5 items)
Actions