Technical Forum

STEP 7 / STEP 7 Lite

Step 7 V5.4 on Windows 7 64 bit platform

Thread Starter: sadrud   Started: 8/17/2010 6:29 AM   Replies: 16

« Previous thread Next thread »
12» Page 1 of 2 (17 items)
  8/17/2010, 6:29 AM
Joined 8/17/2010
Last visit: 9/15/2010
Posts: 1
Rating:
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
 Hi

I am currently using Windows 7 (64 bit operating system). Would anybody let me lnow whether is it possible for me to install Step7 V 5.4 on this operating system.


Regards

Sadrud
Top
  8/17/2010, 6:30 AM
Joined 8/1/2010
Last visit: 3/1/2011
Posts: 10
Rating:
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
 You must wait Step7 V5.5 (11/2010).

A2SVN Company
Top
  8/17/2010, 8:05 AM
Joined 9/28/2005
Last visit: 1/13/2015
Posts: 2927
Rating:
Rated: Excellent [4.03 out of 5 / rated 214 time(s)]. (214) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Hello,

hungass wrote:
 You must wait Step7 V5.5 (11/2010).


Please provide link to the source of information.

Regards,
--------------------------------
Darius
Automation engineer/programmer
Top
  8/17/2010, 3:02 PM
Joined 3/15/2008
Last visit: 1/26/2015
Posts: 6726
Rating:
Rated: Excellent [4.03 out of 5 / rated 690 time(s)]. (690) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
hungass wrote:
 You must wait Step7 V5.5 (11/2010).


V5.5 will be for W7 32 bit, not for 64 bit,
or am I wrong?

Industrieautomation: Softwareerstellung und Inbetriebnahme weltweit.
http://www.ibn-service.com
Top
  8/18/2010, 8:29 AM
Joined 3/21/2006
Last visit: 1/27/2015
Posts: 9931
Rating:
Rated: Outstanding [3.92 out of 5 / rated 1054 time(s)]. (1054) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Hello,

Yes, you are right.Rnf:lblSmileyTooltip_ Only 32 bits.
wrote:

Delivery release 2010-07-26 !
http://support.automation.siemens.com/WW/view/en/42813614
SIMATIC S7, STEP7 V5.5, DATA MEDIUM
INCL. TRIAL LICENSE FOR 14 DAYS,
E-SW, SW AND DOCU. ON DVD, LICENSE KEY ON DVD, CLASS A,
5 LANGUAGES (GE,EN,FR,IT,SP),
EXECUTABLE UNDER WINXPPROF, WINDOWS 7 ULTIMATE, WINDOWS 7 PROFESSIONAL,
REFERENCE-HW: S7-300/400, C7


Best regards,
Hristo Mihalev
Top
  8/18/2010, 9:02 AM
Joined 9/28/2005
Last visit: 1/13/2015
Posts: 2927
Rating:
Rated: Excellent [4.03 out of 5 / rated 214 time(s)]. (214) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
So is it allready out and possible to order ?

Regards,
--------------------------------
Darius
Automation engineer/programmer
Top
  8/23/2010, 5:22 PM
Joined 8/23/2010
Last visit: 8/23/2010
Posts: 1
Rating:
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
I am currently running v5.4 on my windows 7 pro 64 bit 
I installed it  using the windows virtual pc windows xp mode
Top
  8/24/2010, 12:31 PM
Joined 9/28/2005
Last visit: 1/9/2015
Posts: 412
Rating:
Rated: Outstanding [3.68 out of 5 / rated 28 time(s)]. (28) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
sadrud wrote:
 Hi

I am currently using Windows 7 (64 bit operating system). Would anybody let me lnow whether is it possible for me to install Step7 V 5.4 on this operating system.


Regards

Sadrud

According to my latest information you should wait a little longer...
Somewhere around the summer of 2011 is what I heard.
It is obvious that that version is not STEP7 V5.4....

Smurf


"The only difference between a problem and a solution is that people understand the solution."
Top
  8/24/2010, 1:49 PM
Joined 9/28/2005
Last visit: 1/16/2015
Posts: 14
Rating:
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 

Hello,

Last week i've received (and installed) Step7 5.5.
This is what the Help said.

Greetings,

Kees

What's New in STEP 7, Version 5.5?
The following subject areas have been updated:


Operating systems

As of STEP 7 V5.5, the operating systems MS Windows 7 Professional, Ultimate and Enterprise (standard installation) are supported.

Configuring and Diagnosing Hardware

As of STEP 7 V5.5, you can create I-devices from numerous IO controllers.

As of STEP 7 V5.5, you can use the PROFINET shared device function.

As of STEP 7 V5.5, you can assign the IP addresses and device names dynamically.

As of STEP 7 V5.5, you can configure media redundancy for multiple domains.

As of STEP 7 V5.5, you can you can configure the isochronous mode for IO devices.

As of STEP 7 V5.5, you can install hardware updates directly from the "Windows Start menu".

As of STEP 7 V5.5, you can manage user rights for the Web server.

As of STEP 7 V5.5, you can access Web pages of the CPU via a secure HTTPS connection.

As of STEP 7 V5.5, you can configure keepalive times for TCP connections.

As of STEP 7 V5.5, you can download I&M data for more than one module at the same time (using multiselection).
Configuration Changes during Ongoing Operation (CiR)

The restrictions in STEP 7 versions up to and including V5.4 regarding hardware configuration in RUN (CiR) for PROFIBUS when upgrading the STEP version no longer apply in V5.5.

Standard Libraries

As of STEP 7 V5.5, the system functions have been expanded by the addition of SFB104 "IP_CONF" for program-controlled configuration of the integrated PROFINET interface of your CPU.

As of STEP 7 V5.5, the system functions have been expanded by the addition of SFC99 "WWW" for enabling or synchronizing user Web pages.

As of STEP 7 V5.5, the system functions have been expanded by the addition of SFB73 "RCVREC" for receiving data records and SFB74 "PRVREC" for making data records available on an I-device. These SFBs are only valid for S7-300 CPUs.

As of STEP 7 V5.5, the system status list with SSL-ID W#16#xy9C has been expanded. This provides information on the configured tool changer and its tools.

As of STEP 7 V5.5, the following FBs of S7 communication are included: FB28 "USEND_E", FB29 "URCV_E", FB34 "GET_E", FB35 "PUT_E". These are only for S7-300 CPUs and only on connections via the integrated PN interface.

As of STEP 7 V5.5, the following two FBs for open communication via Industrial Ethernet have new names: FB 210 (previous name: "S5FW_TCP") is now called "FW_TCP", FB 220 (previous name: "S5FW_IOT") is now called "FW_IOT".

Report System Error

As of STEP 7 V5.5, you can choose whether or not the status of slaves is evaluated when the CPU starts up.

As of STEP 7 V5.5, the additional texts of messages are displayed or implemented in the "Message Preview", "Print" and "Print Preview" dialogs.

As of STEP 7 V5.5, you can also download blocks generated by 'Report System Error' in HW Config

System diagnostics

As of STEP 7 V5.5, there are two "Diagnostics in Hexadecimal Format" dialogs: one for PROFIBUS slaves and one for PROFINET devices.

Setting the PG/PC Interface

As of STEP 7 V5.5, you can use the USB prommer without needing to install additional software. The required functionality is integrated in STEP 7.

Top
Thank you for this post from:
  8/25/2010, 8:25 PM
Joined 8/29/2009
Last visit: 11/30/2013
Posts: 198
Rating:
Rated: Excellent [4.33 out of 5 / rated 3 time(s)]. (3) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 

Hello !

So does it mean that our Simatic Manager , basically , is a 32-bit application & it will still remain 32-bit application even with the new releases? ........... or did I got it wrong? ..... because many forums (other than this) discuss about 32-bit version Windows & 64-bit version of Windows but we don't hear anything like 32-bit Step7 or 64-bit Step7 version !! 
Regards
Top
12» Page 1 of 2 (17 items)
Actions