Technical Forum

Communication / Networks

Asi Slaves - Significance of K20, K45, K60

Thread Starter: cna   Started: 6/30/2010 6:35 AM   Replies: 1

« Previous thread Next thread »
Page 1 of 1 (2 items)
  6/30/2010, 6:35 AM
Joined 1/15/2010
Last visit: 2/28/2013
Posts: 12
Rating:
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
What is the significance of 20 in K20, 45 in K45 and 60 in K60 in Asi slave devices?



=== Edited by CNagesh @ 6/30/2010 6:37 AM [GMT ] ===


=== Edited by CNagesh @ 6/30/2010 6:36 AM [GMT ] ===


Top
  6/30/2010, 9:03 PM
Joined 12/22/2006
Last visit: 1/25/2015
Posts: 1422
Rating:
Rated: Excellent [4.08 out of 5 / rated 176 time(s)]. (176) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Hello,
K20 are 20 mm wide
K45 are 45 mm wide
K60 are 60 mm wide

The K20 modules are directly mounted without a mounting plate and connected to the AS-Interface using a round cable.

The K60 and K45 modules are mounted with a mounting plate.
The mounting plate is used to receive the AS-Interface flat cables and enables mounting on a wall or standard mounting rail.

Best regards
jklm

Suggestion was helpful? Thanks to rate it.
Top
Page 1 of 1 (2 items)
Actions