Technical Forum

SIMATIC WinCC flexible

How to configure in WinCC Flex 2008 (SP1 HF5) an external tag from PLC which changes every XX seconds (< 60s) as a trigger tag to run the script ?

Thread Starter: Berg   Started: 4/13/2010 8:23 AM   Replies: 1

« Previous thread Next thread »
Page 1 of 1 (2 items)
  4/13/2010, 8:23 AM
Joined 1/17/2006
Last visit: 1/30/2015
Posts: 360
Rating:
Rated: Outstanding [3.62 out of 5 / rated 21 time(s)]. (21) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Darius wrote:
Hello,

Its not possble. Lowest time value using scheduler is one minute. Scheduler can trigger script, but its not capable of handling one second. I think its because running script every second will give hard workload on operating panel. If you still need it then the only possibility is using tag from PLC.


Hello Darius !

  Could you explain me how to configure in WinCC Flex 2008 (SP1 HF5) an external tag from PLC which changes every XX seconds (< 60s) as a trigger tag to run the script ? 

Best regards.

Splitted from WinnCC Flexible ES running a script at every second.



=== Edited by O_Moderator @ 4/13/2010 12:47 PM [GMT ] ===
new subject after splitting


"Educate the children and it won't be necessary to punish the men."
Pythagoras
Top
  4/13/2010, 10:40 AM
Joined 5/24/2009
Last visit: 12/24/2014
Posts: 68
Rating:
Rated: Excellent [5 out of 5 / rated 1 time(s)]. (1) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
In the Tag properties, define a change event which triggers the script... 
Have the PLC change the tag value at a defined time...

cheers,

hans



=== Edited by HansAST @ 4/13/2010 10:41 AM [GMT ] ===


Top
Thank you for this post from:
Page 1 of 1 (2 items)
Actions