Technical Forum

STEP 7 / STEP 7 Lite

Alarme interuption with OB40 in S7300 with 315 2DP

Thread Starter: split 7   Started: 9/11/2006 8:39 PM   Replies: 4

« Previous thread Next thread »
Page 1 of 1 (5 items)
  9/11/2006, 8:39 PM
Joined 9/11/2006
Last visit: 9/12/2006
Posts: 1
Rating:
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
hi

someone can help me about the configuration of alarms interuption.I have same digital inputs that will be programmed in OB40. so i used a digital input ref 

6ES7321-7BH01-0AB0.but no result.

please a help for this problems.

thanks for all.

Top
  9/12/2006, 2:04 PM
Joined 10/10/2005
Last visit: 5/17/2013
Posts: 796
Rating:
Rated: Outstanding [3.37 out of 5 / rated 27 time(s)]. (27) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Hello,

regarding to your inquiry please see our example program in OB40 in the STEP 7 project "P_alarm". Consider you have to adjust the process alarm in the properties of the input modul. See in this case the bmb file "Diag_01".

With best regards
Cicero
Top
  2/9/2007, 9:16 AM
Joined 12/1/2005
Last visit: 2/14/2007
Posts: 3
Rating:
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
>regarding to your inquiry please see our example program in OB40 in the STEP 7 project >"P_alarm". Consider you have to adjust the process alarm in the properties of the input >modul. See in this case the bmb file "Diag_01".

Hi
Could you help me where can I download the programs you mentioned above (P_alarm)
Thanks in advance
Zsolt
Top
  2/12/2007, 8:09 AM
Joined 10/31/2005
Last visit: 5/17/2013
Posts: 2083
Rating:
Rated: Excellent [4.1 out of 5 / rated 197 time(s)]. (197) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
In HW config you should set Hardware interrupt checkbox AND checkbox for each channel you want to call OB40 from.
Top
  2/14/2007, 11:36 PM
Joined 12/5/2005
Last visit: 5/17/2013
Posts: 221
Rating:
Rated: Outstanding [3.56 out of 5 / rated 9 time(s)]. (9) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 

Hi

You can obtain more information about alarm interruption and OB40 in this faq:
http://support.automation.siemens.com/WW/view/en/23657941


Márcio Santos
www.marcioroberto.wordpress.com
Top
Page 1 of 1 (5 items)
Actions