Technical Forum

Decentral Peripherie

ET200s Counter Module 6ES7138-4DA04-0AB0

Thread Starter: Tangowolf   Started: 10/9/2009 5:14 PM   Replies: 2

« Previous thread Next thread »
Page 1 of 1 (3 items)
  10/9/2009, 5:14 PM
Joined 4/29/2009
Last visit: 11/26/2014
Posts: 13
Rating:
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
How do you configure the counter module for the format 12 byte input & 6 byte output option?
All the options in the catelog provide a fixed 8 byte input & 8 byte output configeration.
I am using the new Profinet IO IM 6ES7151-8AB00-0AB0
I need to be able to read the counter frequency as well as the count value.
Please Refererence Entry ID 23378039

Any Ideas?



=== Edited by Tangowolf @ 10/9/2009 5:26 PM [GMT ] ===


Top
  10/9/2009, 9:21 PM
Joined 12/22/2006
Last visit: 1/25/2015
Posts: 1422
Rating:
Rated: Excellent [4.08 out of 5 / rated 176 time(s)]. (176) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Hello,
In the manual I can read this:
=========
Modified user data interface 11 Instead of 8 bytes of input data and 8 bytes of output data, 12 bytes of input data and

6 bytes of output data are used, provided the IM 151 supports this.

The following IM 151 modules support this function:

– IM151-1/Standard order no. 6ES7 151-1AA04-0AB0 and higher

– IM151-1/HF order no. 6ES7 151-1BA01-0AB0 and higher
=======
The IM151-8 is not listed.
I would try as test to configure a decentralized periphery with the listed IMs, to see if this explains your constation.



Best regards
jklm

Suggestion was helpful? Thanks to rate it.
Top
  10/9/2009, 10:35 PM
Joined 11/28/2006
Last visit: 11/23/2009
Posts: 3
Rating:
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
If you go to Entry ID 23378039 in the notes it says that this function is also available in the Profinet -IO IM's. The manual is out of date as it only deals with profibus IM's. The problem is that the hardware manager has no devices that install 12in/6out option ( Profibus or Profinet). This means that we would probably need an additional gsd. outside the standerd ones provided or something else....cry

I am using the IM as a cpu so it is not a remote I/O.



=== Edited by O_Moderator @ 10/10/2009 7:26 AM [GMT ] ===
link edited

Top
Page 1 of 1 (3 items)
Actions