Technical Forum

SIMATIC S5 / STEP 5

CP 1430 TF or TCP

Thread Starter: Desertec   Started: 8/24/2009 11:34 PM   Replies: 3

« Previous thread Next thread »
Page 1 of 1 (4 items)
  8/24/2009, 11:34 PM
Joined 8/24/2009
Last visit: 11/5/2013
Posts: 6
Rating:
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Hello
I am looking for the manual for CP1430 , I 've that this module has obseleted from the the product , even the manual , I tried to get from add-ons ,but it gives  me handbuck (exe)  and I am not able to open .
please if some body have , or could I use CP 1430 TF instead ?
Top
  8/25/2009, 12:21 PM
Joined 7/17/2008
Last visit: 10/25/2013
Posts: 34
Rating:
Rated: Excellent [5 out of 5 / rated 2 time(s)]. (2) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Hello,
Attached you can find the manual
Keep in account that you need the software COM 1430 aswell grin

Regards

Attachment: CP 1430 TCP with NCM COM 1430 TCP_e.pdf  (190 Downloads)

Top
  9/7/2009, 9:35 AM
Joined 8/24/2009
Last visit: 11/5/2013
Posts: 6
Rating:
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
 Hello , Thanks for the manual , I would like to ask one question more? the s5 EPROM for CPs or CPU  could be damaged ? and if it damaged , what will be the outcomes ?
Top
  9/17/2009, 8:40 AM
Joined 3/21/2006
Last visit: 1/29/2015
Posts: 9931
Rating:
Rated: Outstanding [3.92 out of 5 / rated 1054 time(s)]. (1054) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Hello,

Loo at this info about damaging of EPROM:
wrote:

I strongly advise to check the blackening of the EPROM window. If the window isn't covered entirely with a lightshielding tag, it is possible the contents of the EPROM are changed. The construction of these PLC's is open to enable airflow for cooling. But if the air can pass through, so can light! And even a simple TL tube gives enough UV out to damage EPROMs over a certain period of time.


Regards
Top
Page 1 of 1 (4 items)
Actions