Technical Forum

SIMATIC Panel

Can 3 PLC's be connected to 1 HMI panel?

Thread Starter: Bullmeister   Started: 8/18/2009 1:06 PM   Replies: 7

« Previous thread Next thread »
Page 1 of 1 (8 items)
  8/18/2009, 1:06 PM
Joined 8/18/2009
Last visit: 12/3/2009
Posts: 33
Rating:
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Is it possible to connect 3 PLC's to one HMI panel. If so how would it work?

Does Siemens HMI provide redundancy? If so how? Or if not is there any work around?

Regards,

Mike
Top
  8/18/2009, 2:46 PM
Joined 8/18/2009
Last visit: 12/3/2009
Posts: 33
Rating:
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
When I refer to 3 PLC's .... I am trying to work out How Siemens HMI provides redundancy if possible? Any help .. ideas?
Top
  8/18/2009, 4:07 PM
Joined 5/28/2008
Last visit: 6/23/2014
Posts: 900
Rating:
Rated: Outstanding [3.44 out of 5 / rated 128 time(s)]. (128) 
Users with special expertise supervising conferences
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Hello Bullmeister,

you only have to tell us what Panel you use...grinsen

regards
manfred
Top
  8/18/2009, 4:20 PM
Joined 5/28/2008
Last visit: 1/28/2015
Posts: 3288
Rating:
Rated: Outstanding [3.71 out of 5 / rated 598 time(s)]. (598) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Bullmeister wrote:
Is it possible to connect 3 PLC's to one HMI panel. If so how would it work?
Mike


Hello Mike,

Yes it is possible.
You have to connect the three PLCs into one network. Profibus/MPI. Each CPU has an address. And in the WinCC flex. go to controller and define three connections. One for each CPU. Then connect the Panel to the network and it will work.

Regards,

Ayman Elotaify
MISC Egypt
www.miscegypt.com
Top
  8/18/2009, 4:28 PM
Joined 8/18/2009
Last visit: 12/3/2009
Posts: 33
Rating:
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Hi Manfred,

Thanks for the reply. What HMI panel do you suggest for the example. Its all new to me at the moment so I am adjusting to the world of Siemens technology.blush

Here is some more information which I hope will help .... The connection to the HMI panel would be made through the CPU card over Profibus.

I am unsure what type of data is required yet from the PLC's but is there a HMI panel that can except data from both the Profibus network or the Industrial Ethernet.

Thanks for the help. I apologise if my terminology is incorrectly at the moment but with practise I hope to get this correct laugh

Regards,

Mike
Top
  8/18/2009, 4:40 PM
Joined 8/18/2009
Last visit: 12/3/2009
Posts: 33
Rating:
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Cheers Ayman for your answer  laugh

Do you guys know the answer to this  ..... Can Siemens HMI provide redundancy??
Top
  8/18/2009, 9:55 PM
Joined 7/2/2008
Last visit: 1/29/2015
Posts: 812
Rating:
Rated: Excellent [4.26 out of 5 / rated 231 time(s)]. (231) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Hello Bullmeister,

1st of all, welcome to Siemens worldcool.

2nd, I recommend to take a look at,
HMI Panels catalog.

3rd, If I just may add something to what had been mentioned by gentlemen above, it would be,
What is the maximum number of simultaneously active controller connections you can configure for a panel?

4th,
Bullmeister wrote:
Can Siemens HMI provide redundancy??

I'm not sure I fully understand what you mean but if you are asking if Siemens Panels can be connected to redundant controllers (Either software redundancy or H-System), then the answer is YES for sure.
If you ask if panel itself can be redundant, you can have 2 panels communicating to the same controllers and showing the same data (and same screens if you want).
BUT data archives might get different on both panels.

Best regards.

H-H

Edit,
download this video, I hope you will find it useful.
http://support.automation.siemens.com/WW/view/en/21063246



=== Edited by H-H @ 8/18/2009 10:05 PM [GMT ] ===
Video link is added

Top
  8/19/2009, 8:20 AM
Joined 5/28/2008
Last visit: 1/28/2015
Posts: 3288
Rating:
Rated: Outstanding [3.71 out of 5 / rated 598 time(s)]. (598) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Bullmeister wrote:
Cheers Ayman for your answer  laugh

Do you guys know the answer to this  ..... Can Siemens HMI provide redundancy??


Hello Bullmeister,
Actually I am not sure I have understand you correcllty. If your question is a general, I think H-H had ansered you. But you begin your thread by talking about 3 CPUs. So I think you are taling about three different controllers and you want to connect them to one HMI.
In these cases I recommend you to create another thread for two reasons:
1. To make it easy for any body to search for the same subject (i.e. connected HMI to redundant CPUs ).
2. To avoid mis understanding by us.

Any way, Welcome to Siemens.

Regards,

Ayman Elotaify
MISC Egypt
www.miscegypt.com
Top
Page 1 of 1 (8 items)
Actions