Technical Forum

SIMATIC ProTool / ProTool/Pro

HOW CAN I UPLOAD OP17/DP PROGRAM ???

Thread Starter: sundar   Started: 3/5/2009 9:41 AM   Replies: 21

« Previous thread Next thread »
123» Page 1 of 3 (22 items)
  3/5/2009, 9:41 AM
Joined 9/24/2008
Last visit: 1/22/2015
Posts: 97
Rating:
Rated: Excellent [5 out of 5 / rated 1 time(s)]. (1) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
HI TO ALL.

I AM USING SIMATIC PG. IF I UPLOAD OP17/DP PROGRAM TO MY PC THROUGH PROSAVE ITS SHOWING CONNECTION ERROR.

I AM USING MPI CABLE FOR UPLOAD(6ES7 901-0BF00-0AA0) BUT IN PROSAVE SOFTWARE HAVE ONLY ONE CONNECTION SERIAL.


HOW I SHOULD UPLOAD THAT PROGRAM. HMI HAVE 15 PIN PORT. OUR ENGINEERS CONVERT 15 TO 9PIN. I THING THATONE IS WRONG.

CAN ANYBODY SEND CONNECTION DETAILS.

SPEED
Top
Thank you for this post from:
  3/5/2009, 9:49 AM
Joined 4/24/2006
Last visit: 1/27/2015
Posts: 5733
Rating:
Rated: Excellent [4.21 out of 5 / rated 562 time(s)]. (562) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Dear sundar,

You will need cable 6XV1 440-2KH32. laugh

Here is manual: http://support.automation.siemens.com/WW/view/en/1137086
When you look in appendix E, page E-10, you will find lay out of cable. blink

Best regards,

Wizard
Top
  3/5/2009, 9:52 AM
Joined 3/21/2006
Last visit: 1/27/2015
Posts: 9931
Rating:
Rated: Outstanding [3.92 out of 5 / rated 1054 time(s)]. (1054) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 

Hello

Look at C Technical Data OP17 (page 167). togue

regards

Top
  3/7/2009, 3:42 AM
Joined 9/24/2008
Last visit: 1/22/2015
Posts: 97
Rating:
Rated: Excellent [5 out of 5 / rated 1 time(s)]. (1) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 

Hi to all 

I tried with that pin details but i couldn't upload..its showing the following error   
" COULD NOT ESTABLISH CONNECTION CHECK YOUR SETTINGS INTERFACES, CABLES,ETC..)

The  pin connection is
             HMI                       PC
              3                            3
               4                           2
              12                           5

MY prosave version is V7.4.2.0
I also tried with protool 6.0.

What r the other possible for that error. how can i upload the program.

  the HMI have DIP swithches shell i do any modification in DIP swiches.


SPEED
Top
  3/9/2009, 9:12 AM
Joined 4/24/2006
Last visit: 1/27/2015
Posts: 5733
Rating:
Rated: Excellent [4.21 out of 5 / rated 562 time(s)]. (562) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Dear sundar,

I guess you have also on PC side made the connections between 1,6 and 4 
And also connections between 7 and 8. blush

Is OP17 in transfer mode?
If not, you can do it by power off panel. Push and hold the following buttons ESC and 'Button up'
Then power on panel and then you can release buttons. Panel is now in Transfer mode.

Best regards,

Wizard
Top
  3/18/2009, 12:56 PM
Joined 9/24/2008
Last visit: 1/22/2015
Posts: 97
Rating:
Rated: Excellent [5 out of 5 / rated 1 time(s)]. (1) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 

Thanks.
Hi to all.
 I tried many times. But i couldn't upload program.

I am using op17/DP model num (6av3 617-1jc20-0ax1) version 1.03. I download the program using protocol software version 6.0 (COM: 1; BAUD RATE: 38400).

 

The program downloads to OP17/DP without any error. But when I upload the program using same configuration its showing error.

 

I attached the snapshot below.


Attachment: op17.zip  (293 Downloads)

SPEED

Top
  3/18/2009, 2:07 PM
Joined 4/24/2006
Last visit: 1/27/2015
Posts: 5733
Rating:
Rated: Excellent [4.21 out of 5 / rated 562 time(s)]. (562) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Dear sundar,

It's only possible to 'upload' a project from op17 using Prosave. (You can make backup of project)
You can not use the option 'upload' in Protool cry

Remember: You can not change an uploaded project!!sad

Best regards,

Wizard
Top
  3/19/2009, 6:05 AM
Joined 9/24/2008
Last visit: 1/22/2015
Posts: 97
Rating:
Rated: Excellent [5 out of 5 / rated 1 time(s)]. (1) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 

Thanks.
Hi to all.


 I tried many times. But i couldn't upload program.i tried with prosave(v 7.4.1.0) also. when i am using prosave the same error occour.

 

I tried with using  simatic field pg also. using that MPI Port i couldn't download&upload the project. But the OP17/DP cable is Serial port. Is there any other cable need for download the project using PG MPI port instead of serial cable.

 

i attached the prosave error snapshot below.

 


Attachment: prosave.JPG  (202 Downloads)

SPEED

Top
  3/19/2009, 7:39 AM
Joined 5/26/2007
Last visit: 1/3/2015
Posts: 123
Rating:
Rated: Excellent [4.33 out of 5 / rated 3 time(s)]. (3) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
i use this configuration for the cable:

PC (9 pin)       OP17 (15 pin, IF2 port)
2  ->                4
3 ->                 3
5 (GND) ->     5,10,12


it works. before using prosave, turn off OP17, pres ESC and Up key, turn on OP17. wait a second, release the button. the screen will show ready to transfer. run prosave.
Top
  3/20/2009, 11:03 AM
Joined 9/24/2008
Last visit: 1/22/2015
Posts: 97
Rating:
Rated: Excellent [5 out of 5 / rated 1 time(s)]. (1) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Thanks.
I established connection through the above cable configuration using prosave. but i couldn't open from protool software. i want to do modification in upload program means what i should do.

SPEED
Top
123» Page 1 of 3 (22 items)
Actions