Technical Forum

SIMATIC S5 / STEP 5

S5 communication: COM PROFIBUS 3.3

Thread Starter: WernerHimself   Started: 5/29/2006 1:46 PM   Replies: 3

« Previous thread Next thread »
Page 1 of 1 (4 items)
  5/29/2006, 1:46 PM
Joined 5/29/2006
Last visit: 1/22/2015
Posts: 17
Rating:
Rated: Above avarage [3 out of 5 / rated 1 time(s)]. (1) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Import-User-2 wrote:
For this communication the following examples are ready as downloads on the Internet:
http://support.automation.siemens.com/WW/view/de/6711776
DP-connection S7-300 with CP 342-5 (Slave) and IM 308-C (Master) with STEP 7 V4.02
http://support.automation.siemens.com/WW/view/de/6709721
DP-connection CPU 315-2 (Slave) and IM 308-C (Master) with STEP 7 V4.02
http://support.automation.siemens.com/WW/view/de/6556876
DP-connection IM 308-C (Slave) and CPU 315-2 DP (Master) with STEP 7 V4.02
http://support.automation.siemens.com/WW/view/de/6519764
DP-connection IM 308-C (Slave) and CP 342-5 (Master) with STEP 7 V4.02


Für diese Kommunikation stehen im Internet folgende downloads als Beispiel bereit.
http://support.automation.siemens.com/WW/view/de/6711776
DP-Kopplung S7-300 mit CP 342-5 (Slave) und IM 308-C (Master) mit STEP 7 V4.02
http://support.automation.siemens.com/WW/view/de/6709721
DP-Kopplung CPU 315-2 (Slave) und IM 308-C (Master) mit STEP 7 V4.02
http://support.automation.siemens.com/WW/view/de/6556876
DP-Kopplung IM 308-C (Slave) und CPU 315-2 DP (Master) mit STEP 7 V4.02
http://support.automation.siemens.com/WW/view/de/6519764
DP-Kopplung IM 308-C (Slave) und CP 342-5 (Master) mit STEP 7 V4.02



Hi,

Is there also an example available using COM PROFIBUS 3.3?

Thanks in advance



=== Edited by O_Moderator @ 12/14/2010 11:39 AM [GMT ] ===
link edited

=== Edited by CS Moderator @ 5/29/2006 1:52 PM [GMT ] ===
new title

Top
  5/30/2006, 11:32 PM
Joined 1/7/2006
Last visit: 1/8/2015
Posts: 2689
Rating:
Rated: Excellent [4.07 out of 5 / rated 258 time(s)]. (258) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Hi Werner,

Please do you self a pleasure, update to V5.1, i believe that it is possible until Oktobre of this year.

V3.3 have so much trouble that you lose so much time with everything what you are doing, that the price of the up-to-date package is nothing compares to the trouble you will get! sad

It is also not possible to use V3.3 on a newer system, COM PROFIBUS V5.1 with SP2 and hotfixes 1, 2 and 3 may be used with Windows XP SP2 and is working very wel. astonished
(please install the Hotfixes one by one, it is not like the most HF that a higher number have also the lower number in the belly) blush


I hope that the answer will help, if you have still questions, don't hesitate to ask me.

All the best, Late
Never say never, think in solutions, not in trouble......
Top
  6/6/2006, 10:08 AM
Joined 5/29/2006
Last visit: 1/22/2015
Posts: 17
Rating:
Rated: Above avarage [3 out of 5 / rated 1 time(s)]. (1) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Thank you Late,

Where do I get SP2 and the HF's?

Does the software work with a CP5512 profibus card?

Thanks in advance

Werner
Top
  7/8/2006, 6:00 PM
Joined 1/7/2006
Last visit: 1/8/2015
Posts: 2689
Rating:
Rated: Excellent [4.07 out of 5 / rated 258 time(s)]. (258) 
Users with special expertise supervising conferences
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
WernerHimself wrote:
Where do I get SP2 and the HF's?
Does the software work with a CP5512 profibus card?

Hi Werner,
Sorry i give you so late a reply.. blush

Service Pack 2 for COM PROFIBUS V5.1
Hotfix 1 for COM PROFIBUS V5.1
Hotfix 2 for COM PROFIBUS V5.1
Hotfix 3 for COM PROFIBUS V5.1

Every card that is using PG/PC Interface can be used.

I hope that the answer will help, if you have still questions, don't hesitate to ask me.

All the best, Late
Never say never, think in solutions, not in trouble......
Top
Page 1 of 1 (4 items)
Actions