Technical Forum

Communication / Networks

What is the differance between Profinet & Ethernet

Thread Starter: nar   Started: 2/6/2009 11:57 AM   Replies: 4

« Previous thread Next thread »
Page 1 of 1 (5 items)
  2/6/2009, 11:57 AM
Joined 9/30/2008
Last visit: 12/10/2014
Posts: 14
Rating:
Rated: Very Good [2 out of 5 / rated 1 time(s)]. (1) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Dear All,

 I have small question What is the main difference between Profinet And Ethernet

Top
  2/6/2009, 11:48 PM
Joined 5/24/2007
Last visit: 1/15/2015
Posts: 284
Rating:
Rated: Outstanding [3.78 out of 5 / rated 27 time(s)]. (27) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 

Hallo Nar

To be very concise, Profibus protocol sitting on Ethernet Protocols is called as Profinet. It is just that instead of using the RS485 protocol to access the media as in the normal profibus , the  media acess protocols are implemented on Ethernet.

Krish

Top
  2/7/2009, 3:42 PM
Joined 9/27/2006
Last visit: 1/26/2015
Posts: 4952
Rating:
Rated: Excellent [4.23 out of 5 / rated 847 time(s)]. (847) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Hello nar;
If the question is truly important to you, I suggest you look here:
http://www.profibus.com/technology/profinet/overview/

You will find an excellent discussion on the foundations of Profinet, how it uses Ethernet physical layer and protocols to establich connections, how it can be used in 2 different forms at the moment: Profinet-IO and Profinet-CBA.

Hope this helps,
Daniel Chartier



=== Edited by dchartier @ 1/4/2010 1:10 PM [GMT ] ===
Correction of the previous link, did not seem to work anymore

Top
Thank you for this post from:
  2/10/2013, 4:38 AM
Joined 1/17/2006
Last visit: 1/27/2015
Posts: 360
Rating:
Rated: Outstanding [3.62 out of 5 / rated 21 time(s)]. (21) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Hi.

I was looking for info about Profinet and I found a summarized doc but much explanatory and easy for understanding, then I'd like to share with you because it can help someone else.



Best regads,
Berg


"Educate the children and it won't be necessary to punish the men."
Pythagoras
Top
Thank you for this post from:
  2/15/2013, 12:06 PM
Joined 9/8/2009
Last visit: 1/26/2015
Posts: 746
Rating:
Rated: Outstanding [3.84 out of 5 / rated 50 time(s)]. (50) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
The major difference is hardware layer of  slave devices. While the master (PC or PLC) uses a standard NIC hardware, slave devices are using special hardware ASIC FPGA or DSP to route packets from one port to other.
They also need to change data on the fly, while receiving data on one port they exctract data and change/route forward on the fly, you will notice that profinet has some delay for each device.  
A profinet master is cheap running with ordinary NIC, while slave device is very expensive.  
Top
Page 1 of 1 (5 items)
Actions