Technical Forum

SIMATIC ProTool / ProTool/Pro

ProTool 6.0 SP 3 with Windows XP SP3

Thread Starter: NewTech   Started: 10/10/2008 1:24 PM   Replies: 4

« Previous thread Next thread »
Page 1 of 1 (5 items)
  10/10/2008, 1:24 PM
Joined 2/23/2007
Last visit: 1/28/2015
Posts: 66
Rating:
Rated: Outstanding [4 out of 5 / rated 1 time(s)]. (1) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Hi all,

I have ProTool v 6.0 SP 3 installed on my pc with Windows XP SP 3, but when I try open an application created on this version have an error:

"Error on converting OID 5 == OID_POB_CTDRIVER_MANAGER. Please contact the manufacturer."

"Unexpected file format"

Atached images.

I already try:

  • Complete Deinstallation of ProTool/Lite, ProTool resp. ProTool/Pro under Entry-ID: 18697689
  • Installation details regarding ProTool Lite, ProTool and ProTool/Pro under Entry-ID: 18695605
But still have problems on my applications.

Anybody have any ideia to solve this problem???

Thanks for any help
Marcelo Oliveira

Attachment: ProTool_Erro_1.JPG  (76 Downloads)

Top
  10/10/2008, 3:29 PM
Joined 4/24/2006
Last visit: 1/30/2015
Posts: 5736
Rating:
Rated: Excellent [4.21 out of 5 / rated 564 time(s)]. (564) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Dear NewTech,

I guess you have seen this faq: http://support.automation.siemens.com/WW/view/en/13396711

That message comes when protool project was saved in later version of Protool. But Protool v6.0 + sp3 is latest. sad

Perhaps Servicepack 3 for Windows XP is the problem. Here is compatibility between Protool and Windows: http://support.automation.siemens.com/WW/view/en/8795248  There is no mentioning about Windows XP + sp3. cry

Best regards,

Wizard
Top
  10/11/2008, 2:16 PM
Joined 5/28/2008
Last visit: 2/1/2015
Posts: 3290
Rating:
Rated: Outstanding [3.71 out of 5 / rated 599 time(s)]. (599) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Hi NewTech,
It's a very strange thing I have never seen. But try to use Windows XP+SP2 with your protool.
I didn't seen this problem as While I was using Windows XP+SP2 and protool, I moved to winCC flexable. And then I moved to Windows XP+SP3 with winCC flex. No more work with protool. Any way, just try to use Windows XP+SP3 or try to use WinCC flexable. You can migrate the protool project to WinCC flexable project easily and without instaling Protool.
Regards,

Ayman Elotaify
MISC Egypt
www.miscegypt.com
Top
  10/13/2008, 7:40 PM
Joined 8/17/2007
Last visit: 10/3/2013
Posts: 488
Rating:
Rated: Excellent [4.31 out of 5 / rated 35 time(s)]. (35) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Yes XP SP3 is known to give trouble with Protool.

Here is the info from MS, how to uninstall SP3

http://support.microsoft.com/kb/950249

Jomy M Jose
Jacobs Engineering Group Inc.
111 Corning Rd., Suite 200
Cary, NC 27518, USA
Top
  11/17/2011, 8:05 PM
Joined 11/17/2011
Last visit: 11/22/2011
Posts: 2
Rating:
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Hi New Tech,

I have had the same problem, and it was not solved by uninstaling XP SP3 or by reinstalling the PC with a brand new Windows XP SP2 ...

It was solved by reinstalling Step 7 V5.4 with it´s SP 3.1 - and nothing more.

I think that the problems occurs from the upgrade packs for Step 7 SP4 & SP5.

Try to reinstall Step 7 without the additional upgrades, and then install Protool. After that you can install the Step 7 upgrades.

Richard. Rnf:lblSmileyTooltip_goal
Top
Page 1 of 1 (5 items)
Actions