Technical Forum

Communication / Networks

Fanuc robot R-J3 controller

Thread Starter: MrBus   Started: 5/1/2012 2:19 PM   Replies: 12

« Previous thread Next thread »
«12 Page 2 of 2 (13 items)
  5/11/2012, 3:37 PM
Joined 8/31/2010
Last visit: 5/24/2013
Posts: 1257
Rating:
Rated: Outstanding [3.88 out of 5 / rated 104 time(s)]. (104) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
MrBus wrote:
The  R30iA mate controller is not availible in PN.
Has anyone used the KP1200 Profinet to the TCP/IP proto from AB. the KP1200 can comm to the AB tcp/ip, how about the fanuc robot,  it does tcp/ip to a AB controller?



Hello MrBus,
I hope you have mentioned about the comfort panel KP 1200. Correct me if I'm not right. Allen-Bradley EtherNet/IP is supported by Comfort Panels. But still can you pls put your question in different words, I'm not able to get it clearly.

Like it? Rate it!
Top
  5/16/2012, 4:23 PM
Joined 1/5/2011
Last visit: 5/1/2013
Posts: 13
Rating:
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Thanks for your interrest.I wish to transfer tags data from my KP1200 to the Fanuc R30 controller via Profinet.
Has anyone done this?
Top
  5/16/2012, 6:45 PM
Joined 8/31/2010
Last visit: 5/24/2013
Posts: 1257
Rating:
Rated: Outstanding [3.88 out of 5 / rated 104 time(s)]. (104) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
MrBus wrote:
Thanks for your interrest.I wish to transfer tags data from my KP1200 to the Fanuc R30 controller via Profinet.
Has anyone done this?

Hello MrBus,
PROFINET can be used only for the below mentioned in the Comfort Panel.
1. Function keys or buttons are configured as PROFINET IO direct keys in the project
2. The backlighting of the HMI device is to be controlled with PROFIenergy

Like it? Rate it!
Top
«12 Page 2 of 2 (13 items)
Actions