SIMATIC TDC, FM458, T400
about SIMADYN MACRO
Thread Starter: DUTTA Started: 5/29/2008 4:19 PM Replies: 3

5/29/2008, 4:19 PM
|
Joined 2/26/2008
Last visit: 3/14/2013
Posts: 97
Rating:
(0)
|
(0)
|
Dear Expert,
I m currently working on 16bit Simadyn Processor which contains MS31 Eproms. I got the backup of program for these processors by using RCOP.
But inside the program it shows one block which I think is a macro.
Can any one tell me how to read this macro. The library what I have, is older one shows year 1992 and then after according to my client these macro might have changed in 1997. So I worry about that I cant complie this code once again.
Now my task is to recomplie these code from MS31 EPROM using RCOP and generate the backup means prepare another MS31 EPROM.
Can any one tell in this case how can I create another backup MS31 EPROM by reading existing EPROM???
with best regards, Dutta
|
|
|
|

5/30/2008, 6:03 PM
|
Joined 8/31/2005
Last visit: 5/22/2013
Posts: 983
Rating:
(122)
|
(0)
|
I m currently working on 16bit Simadyn Processor which contains MS31 Eproms. I got the backup of program for these processors by using RCOP. But inside the program it shows one block which I think is a macro. So you successfully copied the content of the EPROM and EEPROM to files? Where do you stuck, by recompiling the PN, MP or FP? Or do you have a unknown block in a FP-Listing?
In STRUC V3 there is no Macro possible. But in all STRUC versions you can have user libaries. This libaries are a extension that allow customers to use own function blocks. You have to ask the owner of a libary for the required files.
Can any one tell me how to read this macro. The library what I have, is older one shows year 1992 and then after according to my client these macro might have changed in 1997. So I worry about that I cant complie this code once again. You are right, if the libary does not match to the STRUC version you can not compile. But I think, external libaries may be used while the last digit of the version of STRUC changes, e.g. it works for V3.2.x
Now my task is to recomplie these code from MS31 EPROM using RCOP and generate the backup means prepare another MS31 EPROM. Can any one tell in this case how can I create another backup MS31 EPROM by reading existing EPROM???. RCOP ist the only way. If you are lucky, there may be a additional way to make a backup: If the chips of the MS31 are not soldered but have socklets, you may use a (E)EPROM Reader/Programmer and copy chip by chip.
mfG / Best Regards
Dirk
|
|
|
|

5/30/2008, 7:43 PM
|
Joined 2/26/2008
Last visit: 3/14/2013
Posts: 97
Rating:
(0)
|
(0)
|
Dear Miami,
Thank you very much for the reply.
I will try to find the autor of the library, but I am doubtful that he might have retired as it was very older group.
I have also cheked the MS31 EPROMs and yes its not soldired so I can remove those. can u tell me exact procedure in details how to copy the chips from one MS31 to another?
with best regards, Ankur
|
|
|
|

6/12/2008, 5:47 PM
|
Joined 8/31/2005
Last visit: 5/22/2013
Posts: 983
Rating:
(122)
|
(0)
|
I have also cheked the MS31 EPROMs and yes its not soldired so I can remove those. can u tell me exact procedure in details how to copy the chips from one MS31 to another? No, I never had to do it, but it should not be a problem to make a 1:1 copy of the chips with the software with is used for a "chip burner"
mfG / Best Regards
Dirk
|
|
|
|
Actions