Technical Forum

SIMATIC TDC, FM458, T400

@DU3 block

Thread Starter: DUTTA   Started: 3/21/2008 3:58 PM   Replies: 2

« Previous thread Next thread »
Page 1 of 1 (3 items)
  3/21/2008, 3:58 PM
Joined 2/26/2008
Last visit: 3/14/2013
Posts: 97
Rating:
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Dear Expert,

I want to use Dust 3 protocol in PM16 processors. For that I have configured a sample program in STRUC L V4.2.7

In that project I configure master program with 1 PM16 processor, MS41, and  two Serial Interface.

In Master program configuratoin when I m trying to call @DU3 block I can not.
It give me the message Name defination is defective.

Can u tell me what should I do to call DUST 3 block?

regards,
Top
  3/26/2008, 1:43 PM
Joined 8/31/2005
Last visit: 5/24/2013
Posts: 984
Rating:
Rated: Outstanding [3.85 out of 5 / rated 122 time(s)]. (122) 
Users with special expertise supervising conferences
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
I'm not shure, because it changed from STRUC 3 to STRUC 4.

But I think in STRUC 4 you have to call the @DU3 in the FP-SEND (in a tasktime between 32 and 256 ms)
In the masterprogram you only define the hardware.

I



=== Edited by miami @ 3/26/2008 1:45 PM [GMT ] ===



mfG / Best Regards

Dirk
Top
  3/26/2008, 1:53 PM
Joined 2/26/2008
Last visit: 3/14/2013
Posts: 97
Rating:
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Dear Miami,

Yes I have placed @DU3 block in SEND-FP and got successful complied my programe.

thanx for the help

regards,
Top
Page 1 of 1 (3 items)
Actions