Technical Forum

LOGO!

connect LOGO! to PC under Windows se7en OS

Thread Starter: realpower_ir   Started: 7/30/2012 11:22 PM   Replies: 9

« Previous thread Next thread »
Page 1 of 1 (10 items)
  7/30/2012, 11:22 PM
Joined 11/30/2008
Last visit: 3/17/2013
Posts: 28
Rating:
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 

 

Dear Expert Mr. Marcjan,

 

I hope it finds you well. 

 

I have a same problem like that. My problem is to connect LOGO! to PC under Windows se7en OS. I use the diver for USB cable which be delivered by setup.exe (LOGO! Comfort Ver 7.0.30). It connects just one time after windows boot-up and suddenly it loses its connection with LOGO! by the same upper mentioned error message. Always at online test mode. And most of the time there is no chance to connect.

I am sure my cable is right. Because with this version of LOGO! Comfort, under Windows XP! it works continuously. Even without any disconnection.

I would very happy if you let me know, why.

 

Best regards,

 

Yours Reza

 

P.S. Can I get your answer here? Or I should make a new thread?

 




=== Edited by O_Moderator @ 7/31/2012 11:17 AM [GMT ] ===
new subject after splitting from connecting Siemens Logo! with PC

Top
  7/31/2012, 7:36 AM
Joined 4/22/2010
Last visit: 5/17/2013
Posts: 3186
Rating:
Rated: Excellent [4.11 out of 5 / rated 295 time(s)]. (295) 
Users with special expertise supervising conferences
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Hello,

When you say only with online test, you mean up/down load is working correct?
What Logo you have there?
Can you make a printscreen of Help---->About----> system info.
Perhaps a new version of Java must be installed, have no Win 7 here to check some settings.
With some Logo i had some trouble with Online test too, but after upload it was o.k.


Regards,

Marcjan

Problem solved?
Please let us know!

Please no technical questions by PM, use the forum!
Top
Thank you for this post from:
  7/31/2012, 8:04 AM
Joined 7/24/2006
Last visit: 5/16/2013
Posts: 1823
Rating:
Rated: Outstanding [3.68 out of 5 / rated 216 time(s)]. (216) 
Users with special expertise supervising conferences
Rated: Outstanding [4 out of 5 / rated 1 time(s)]. (1) 
Hi,

try to set the right LOGO! in the SW you have realy connected.

Lots of user have programms created for older LOGO!. They open the old program edit and download in lots of cases to a newer LOGO!. So they forget to select the right LOGO! also in the Program. Download works in lots of cases but online test doesn't work

If an actual LOGO! 0BA6 is used, then you have to select LOGO! 0BA6 ES3 as LOGO!.
Otherwise the Online test will not work. Same with 0BA7. If a LOGO! 0BA7 is connected and you want to start online Test be sure to have LOGO! 0BA7 selected as LOGO! HW.

Hope this helps
Top
Thank you for this post from:
  7/31/2012, 8:24 AM
Joined 7/26/2012
Last visit: 4/29/2013
Posts: 25
Rating:
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
i also have the same concern. i have ob7 (6ED1 053 1FB00 0BA7) and laptop. i cannot communicate logo. i connected logo using ethernet cable. my logo has it own supply.
please help me connect or how to configure ob7 to connect with laptop loaded with W7

Just Listen... and Read my Eyes
Top
Thank you for this post from:
  7/31/2012, 8:56 AM
Joined 4/22/2010
Last visit: 5/17/2013
Posts: 3186
Rating:
Rated: Excellent [4.11 out of 5 / rated 295 time(s)]. (295) 
Users with special expertise supervising conferences
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Hello,

Have a look at attached document to setup the Logo and Logosoft.

Document can also be found in Logo application Examples

Make sure your IP is in the same range (only last digit may be different) and Subnet is the same.

Regards,

Marcjan

Attachment: EN_Connection_LOGO!0BA7-PC.pdf  (53 Downloads)



=== Edited by Marcjan @ 7/31/2012 8:59 AM [GMT ] ===



Problem solved?
Please let us know!

Please no technical questions by PM, use the forum!

Top
  8/2/2012, 11:22 PM
Joined 11/30/2008
Last visit: 3/17/2013
Posts: 28
Rating:
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 

Dear Expert Marcjan,

 Thank you very much in advance for your attention and replying.

 Very kindly, I am very sorry if my previous comment wasn’t enough clear to understand. I didn’t say “only at online test”. My major problem is “most of the time I can not get any connection to LOGO! (any version that I’ve used such as OBA5, OBA6 and still I haven’t use of OBA7) by LOGO! Comfort software under Windows se7en O.S.

 For first step of work (getting connection to LOGO! under Windows se7en) I should several time try to do connect for uploading or downloading my prog*.lsc. And if I be lucky to make a connection, next, it will be terminated by running “online-test mode” after approximately a minute certainly.

 But, as I already said, if I work under Windows XP! O.S. definitely every thing goes well with my all hard wares.

 That sounds strange!

 I appreciate you for your very friendly supporting and guidance.

 Best regards,

 Reza

 

 P.S: Special thanks to O_Moderator for creating this thread.


Attachment: MySysInfo.jpg  (30 Downloads)



=== Edited by realpower_ir @ 8/2/2012 11:25 PM [GMT ] ===



Top
  8/2/2012, 11:41 PM
Joined 11/30/2008
Last visit: 3/17/2013
Posts: 28
Rating:
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 

Hello Helmut,

When I was working on my program (with LSC extention) under Windows XP! O.S. everything was all right (up&downloading and online test mode)

 Is this your remedy just for solution in Windows se7en?

 Or it is a general trick?

 Thank you

Top
  8/17/2012, 11:37 PM
Joined 11/30/2008
Last visit: 3/17/2013
Posts: 28
Rating:
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Dear Sirs,

I hope it finds you very well.

I am really in trouble with Windows se7en, as I already explained in this thread.

Is any recommand?

All suggestions are welcome.

Best regars,

Reza
Top
  8/20/2012, 9:13 AM
Joined 5/3/2011
Last visit: 4/2/2013
Posts: 461
Rating:
Rated: Outstanding [3.89 out of 5 / rated 46 time(s)]. (46) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Did you try to reinstall the driver? If no, then uninstall the LOGO! USB Driver, download the driver here and install it new.

Regards,
Mc Muffin
Top
Thank you for this post from:
  8/20/2012, 9:45 AM
Joined 11/30/2008
Last visit: 3/17/2013
Posts: 28
Rating:
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Dear Mc Muffin,

Thank you very much in advance for your kind reply.

I did. It was my first step on remedy way.

Best regards,

Reza
Top
Page 1 of 1 (10 items)
Actions