Technical Forum

SIMATIC S5 / STEP 5

SINEC NCM COM V5.01

Thread Starter: stanlist   Started: 8/28/2006 4:36 AM   Replies: 4

« Previous thread Next thread »
Page 1 of 1 (5 items)
  8/28/2006, 4:36 AM
Joined 8/28/2006
Last visit: 8/28/2006
Posts: 1
Rating:
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 

Good day to all,

can anyone please advice me on following menthod
1. where can I get the SINEC NCM COM V5.01 installation file?
2. If i do have the installer, how to setup?
i do some kind of SINEC NCM installer, however i always stuck on the following screen (please find the attachment: CP1430.gif)

Thanks
regards
stanlist


Attachment: cp1430.gif  (85 Downloads)

Top
  8/28/2006, 11:11 AM
Joined 2/14/2006
Last visit: 5/6/2013
Posts: 5798
Rating:
Rated: Outstanding [3.96 out of 5 / rated 358 time(s)]. (358) 
Rated: Excellent [5 out of 5 / rated 1 time(s)]. (1) 
Hello,

one question, it seems that you do not use a FDD for the Installation.
As I know the NCM COM 1430 TCP a bit I would recommend the use of a FDD really strongly. It may sound a bit strange, but this Software is based upon Software that is over all based on PCPM OS or MS-DOS. You should really use a FDD, a installation from a Network drive usually will not work.

Best regards

J_Bell
Top
  1/23/2008, 2:38 PM
Joined 11/23/2007
Last visit: 8/1/2011
Posts: 22
Rating:
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Hallo J_Bell
I had the same problem, but i have solved it by your remedy. It's abaout the FDD (Floppy Drive). It works when you install it from a floppy dirve.  
Thanks For your helpslaugh

DerJunge



=== Edited by derjunge82 @ 23.01.2008 15:05 [GMT ] ===


Top
  8/9/2012, 12:34 PM
Joined 5/11/2006
Last visit: 3/3/2013
Posts: 22
Rating:
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Hi,

Same problem here. Could anyone tell me if this will work with a USB floppy drive please? I've tried a virtual floppy drive but it didn't work.

Many Thanks.
Top
  8/9/2012, 1:33 PM
Joined 5/11/2006
Last visit: 3/3/2013
Posts: 22
Rating:
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Hi, did get it to work with the virtual floppy. Just had to put all the files directly in the virtual floppy, not within a folder in it.
Top
Page 1 of 1 (5 items)
Actions