Technical Forum

DC converters SIMOREG

supply

Thread Starter: conical   Started: 8/8/2012 5:41 AM   Replies: 1

« Previous thread Next thread »
Page 1 of 1 (2 items)
  8/8/2012, 5:41 AM
Joined 2/7/2006
Last visit: 6/10/2013
Posts: 16
Rating:
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Dear experts

I have a 6RA70 with MLFB 6RA7078-6DS22-0-Z-=L04+K01+K11+G94,
INPUT: 3-PHASE AC 400V, 233A

my question is :
with option L04, 6RA70 device can only feeded with a power supply of voltage range 15V - 85VAC?

or voltage range 15V - 400VAC?

what is main function for option L04, where can I find a detail descrition for this option?


many thanks

Attachment: D:\Users\cn1jh160\Desktop\voltage range.jpg  (8 Downloads)

Top
  8/9/2012, 7:05 AM
Joined 8/25/2006
Last visit: 6/18/2013
Posts: 909
Rating:
Rated: Excellent [4.21 out of 5 / rated 86 time(s)]. (86) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Hello.
With L04 you can supply only 15-85VAC. With this option the power interface board is different (C98043-A7002-L41 instead of standard C98043-A7002-L1).
Main function is work at low voltage. Look at neighboring thread.
Top
Page 1 of 1 (2 items)
Actions