Technical Forum

Low-Voltage Power Distribution and Installation Technology

Read some values from PAC3100 with et200s

Thread Starter: juriskg   Started: 8/6/2012 4:42 PM   Replies: 2

« Previous thread Next thread »
Page 1 of 1 (3 items)
  8/6/2012, 4:42 PM
Joined 5/4/2012
Last visit: 4/13/2013
Posts: 4
Rating:
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Hi,

I have task to read some values from PAC3100 with et200s. But i don't have a clue how it should be done. Can you maybe describe me what should i do. I had assignment to create my own PID regulator, so i could manage water level. This part is finished. But now i have part for reading energy consumption. In this part i have lack of knowlege. Can you maybe help me. It is my master degree work.

Thanks, and BR
Marko



=== Edited by Blue Moderator @ 8/6/2012 9:08 PM [GMT ] ===
Splitted from How to read 64 bit floating value from PAC3100 and renamed

Top
  8/6/2012, 10:24 PM
Joined 9/27/2006
Last visit: 5/24/2013
Posts: 3948
Rating:
Rated: Excellent [4.15 out of 5 / rated 620 time(s)]. (620) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Hello Marko;
How familiar are you with Modbus RTU? The Sentron PAC 3100 has a RS-485 interface dedicated to Modbus RTU exchanges, so best we start with that clarification. For your general information (or some quick refreshment) here is an excellent post from our forum friend smiffy explaining the basics of Modbus RTU:
Modbus General Description  
Also, what level of experience do you have with Siemens programming and PLCs? Knowing this will help us determine how we can help you best.

Just for starters, you will need a serial communication module for your ET 200S CPU; this would be a 1SI module; the model shown here is setup for Modbus RTU, using RS-485:
http://support.automation.siemens.com/WW/view/en/20270713

Here is a link to the manual for the 1SI module:
ET 200S 1SI manual

and here is a link to the PAC 3100 manual, including a Modbus mapping (available variables for Modbus exchanges, including the offset address of each one; see the appendices):
Sentron PAC 3100 manual


Finally, here are 2 sample programs that might help you out in your project:

PAC 3100 and Modbus sample program for the 1SI module :https://www.automation.siemens.com/WW/forum/guests/PostShow.aspx?HTTPS=REDIR&PostID=367554&language=en
 
PAC 3100 and sample program for CP 441-2 (S7-400):
Modbus communication with Sentron PAC3100 RS485 Module to S7 400 Communication with two quary sample program   



Hope this helps,
Daniel Chartier




=== Edited by dchartier @ 8/6/2012 10:26 PM [GMT ] ===


Top
  8/7/2012, 8:26 PM
Joined 5/4/2012
Last visit: 4/13/2013
Posts: 4
Rating:
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Hi,

I already have listed what you sent to me. Main problem is how to comunicate with PAC3100. I am using TIA, and ET200s as i mentioned, and all examples and explanations are made either in step7, or for S7-1200. So with my present knowledge i can't use those examples since i don't know how.

Thanks and Best Regards,
Marko.
Top
Page 1 of 1 (3 items)
Actions